This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C Hibernation Question

Expert 1070 points

Hello,

I am interested in using the hibernate mode on the TM4C devices because of the super low power.  I would like to retain variables in memory during the period of hibernation.  Is this even possible?  I believe the VDD3ON mode will hold I/Os for me, but can't figure out the approaches for retaining memory.  Perhaps an external piece of memory?

Thanks for your help.

LER

  • Hello LER

    In VDD3ON mode only IO state is preserved. The only place that can retain data is the Hibernate Battery Back RAM which is a set of registers.

    Regards
    Amit
  • Hello Amit,

    So if I use Hibernation mode, with VDD3ON mode, I would like to maintain a chunk of battery backed SRAM that would maintain my program and heap space while the processor is hibernating.  Then, when the processor reboots, I could load the processors registers back up from same EEPROM (or SRAM) and begin executing from where I gracefully hibernated before.

    Does this sound like it would work?  What other considerations should I be making?

    Thank you.

    LER

  • Hello Ler,

    No. The Battery back RAM is a set of registers only. The main SRAM would be lost. If you want to maintain the SRAM contents then Deep Sleep with voltage scaling and frequency scaling would be correct low power state.

    Regards
    Amit