Other Parts Discussed in Thread: HALCOGEN
Hi,
I have a simple SPI application built in the IAR development environment. I am using mibspi1. The halcogen-generated
function mibspiInit() is getting hung here:
/** - wait for buffer initialization complete before accessing MibSPI registers */
/*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
while ((mibspiREG1->FLG & 0x01000000U) != 0U) <---------------------------------------------------------
{
} /* Wait */
When examining the mibspi1 registers it appears that any register that has not been written to up to this point has the value 0xCDCDCDCD
which does not seem correct.
I have attached the halcogen config file as well as a register dump.0842.mibspiRegs.logAny ideas what might be going on?
Victor