This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI 14 pin to ARM 20 pin converter

Hello.

We have a XDS100v2 Jtag probe with a TI 14 pin connector, that we used a TMS320F micro-controller.

Now we received, from a partner of ours, a board that they developed with a TMS570LS on it and we need to connect to it to upload a new software version.

On the board an ARM 20 pin connector is available to connect the probe.

I read on XDS100v2 specifications that it can be also used on all ARM micro-controllers, that is the case of TMS570LS.

Now the pin names for the TI 14 and the ARM 20 connectors are exactly the same and only the pinout changes.

Except for the pinout, are the TI 14 and the ARM 20 connectors fully compatible?

I mean: if I build a cable that converts the pinout from the TI 14 to the ARM 20, will it work?

Thank you very much.

Best regards.

          Daniele