Other Parts Discussed in Thread: TM4C1294NCPDT
I looked through the datasheet but was unable to find a solid answer.
I am using the 16 MHz PIOSC on the TM4C1294NCPDT. I originally had a 25 MHz crystal to run at 120 MHz, but missed the RBIAS errata so am forced to use the internal oscillator.
- The VCO must be configured to 320 MHz when using PIOSC, correct?
- The maximum operating frequency must be a divisor of VCO. I have it configured at 80 MHz but can it run at 160 MHz?
Thanks,
Dan