Other Parts Discussed in Thread: HALCOGEN
I have one of the TMS570LC43x development kits. I worked through the PWM & eCAP example in HalCoGen and was able to get this fully functional using PWM1 and eCAP1. I then attempted to extend this to utilize eCAP5 (what I will use in my final application) and I have not been able to get the interrupt to fire. I think I got everything configured correctly in HalCoGen but obviously I am missing something. I connected the PWM1 to pin 'H18' on the development kit and I can confirm the PWM output is getting to the pin with an o-scope. Any suggestions on what I have not connected up correctly to get this interrupt to fire would be very much appreciated. Attached I have included the project I am trying to get to work.
I am using CCS V: 6.1.0.00104
I am using HalCoGen V: 04.05.01