This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-SENSHUB Sensor Hub BoosterPack air mouse problem



Hi ,

I just tried the air mouse example using the TM4C123GXL and the BOOSTXL-SENSHUB.. The LEDs are as follows: green on the TM4C, solid blue and rapidly flashing red on the booster pack. The left and right buttons on the TM4C work as intended as mouse buttons. However, rolling or moving the board slowly or rapidly has no effect on the muse pointer. I am taking an introductory embedded systems class as an undergrad so my knowledge of microcontrollers is quite limited so please forgive any dumb questions I might ask :)

I am using a Windows 8.1 laptop.

I am not sure what is wrong. The device appears to be fine in device manager under HID. One question, I assume I inserted the pins on the MC correctly into the booster pack. It is oriented correctly and all pins were inserted, As I said previously, the insertion must be fine since the LEDs etc. are as expected.

Thanks for any help.

--

John