This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Timer CCP edge counts very slow in debug and stops counting when edges count jumps 150Hz - 200Hz.

Guru 55923 points


Timer is set in edge count mode with an interrupt on match count to update match count value as to increment the timer count value with the number of edges per seconds then converted into RPM to display the speed. The timer block shows 32kHz input into the CCP0/1 pins so it seems it should not have trouble at 202Hz.

 If the GPTM timer re-load TnILR value is kept 4 edges ahead of the TnMatchCHR value the timer counts UP and auto reloads at 107hz if TnMatchCHR is unchanged. However a sudden speed up in edge count to 150Hz and the timer appears to quickly stop counting well below the value in TnILR until the edge counts once again become 107Hz. Setting the TnILR load value very high to 1616 edges or { 2 pulses per revolution being 404 pulses x 4 edges @202Hz = 6300 RPM}. 60RPS=60Hz/2PPS/Revolution=30PPS or 1616 edges / 30 = 53PPS at 6300 RPM. So the math formula works back words to prove edge count to RPS to RPM.

Only incrementing the match CHR by 4 edges each interrupt cycle has a worse effect to completely stop the match CHR interrupt. Allowing the count to climb and keeping 4 edges between TnILR - MatchCHR as the count value climbs a very slow increments in debug that doesn't match the realtime edges per-second. The debug values appear to change in 1 second intervals and stops counting within few seconds upon a forces jump in fan speed. The best count achieved is from 1-8 edges per interrupt cycle and renders 253 RPM readout at 107Hz. Seemingly impossible to count edges any faster at higher frequency.

Food for thought 1616 edges per revolution at 6300 RPM = 202Hz square wave being 96,960 edges per minute. According to some folks 6300 RPM appears to resolve to 52.5 pulses per-second so the taco signal is running a bit hot on this fan.

Why is capture edge count not playing nice?

  • Hello BP101

    Which direction of frequency change does the stop count happen in 150 to 200 or 200 to 150Hz change?

    Regards
    Amit
  • Hi Amit,

    The exact frequency is unknown, only guessing is 150 - 200Hz. Stops counting when ever TnMatchCHR has been reached. Then from debug point of view the timer fails to use the interrupt updated reload value in TnILR either being a static span of 1616 edges or if in an incrementing 4 edge gap band kept between TnILR/MatchCHR. Thus counting up to 404 adding (+= 0x0004 to TnILR and or MatchCHR) based on factoring TnV and TnR (if < 202 edges) calculations done in the interrupt cycle. In a 4 count edge gap method the timer cycle seems to go a bit further before it hangs. Even if using PreScaler with much higher initialized load/match values they are never matched in the up count so It doesn't appear to be a wrapping count issue.