This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

No MibSPI1 RAM parity error was flagged to ESM

Other Parts Discussed in Thread: RM48L952, HALCOGEN

Hello, 

I have received a new dev board kit RM48L952 rev C. 

to test the board I have generated the drivers usign HALCOGEN 04.05.01. I have enabled several peripheral, and I have set the Ram parity for the MIBSPI 1, 3, 5.

In the file sys_SelfTest I have put a while(1) in the function selftestFailNotification in order to catch a fault if a selftest fails

When running the target, the mibspi1ParityCheck function fails, "No MibSPI1 RAM parity error was flagged to ESM". If I comment out the mibspi1ParityCheck, I can see that the other mibspi3ParityCheck and mibspi5ParityCheck run correctly.

I have tested this with another board with revision B and there is no error reported for the mibspi1.

Is it enough testing to say that there is a problem with the board on the mibspi1 ?

thank you.

Brice