Other Parts Discussed in Thread: LM3S617, LM3S818
Hello,
I am trying to debug a problem with a Stellaris LM3S617 micro, but have now run into another problem. When I attempt to connect to the micro via JTAG I get the following message:
"CORTEX_M3_0: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.14.5)"
JTAG emulator: Spectrum Digital XDS200USB
CCSv5: version 5.5.0.00077
I have tested the JTAG connection using the "Test connection" button in the .ccxml editor and no errors were reported.
I have tried this with 2 different XDS200USB emulators and 1 Spectrum Digital 560v2 STM emulator. All give the same error message.
The micro has power (3.3V on pin 7). I've tried various JTAG CLK speeds, but get the same error message.
Any ideas, or is this micro no longer any use to anyone?
Cheers,
Ian