Other Parts Discussed in Thread: SYSBIOS
Good day,
I want with Timer2, the Timer_B throws me a hardware interrupt.
The code is simple:
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER2);
TimerClockSourceSet(TIMER2_BASE, TIMER_CLOCK_SYSTEM);
TimerConfigure(TIMER2_BASE, TIMER_CFG_B_PERIODIC);
TimerLoadSet(TIMER2_BASE, TIMER_B, 0xFF);
TimerIntEnable(TIMER2_BASE, TIMER_TIMB_TIMEOUT);
IntEnable(INT_TIMER2B);
IntMasterEnable();
TimerEnable(TIMER2_BASE, TIMER_B);
and in .cfg file I created a hardware interrupt having number 40:
var hwi0Params = new Hwi.Params();
hwi0Params.instance.name = "hwiTimer2";
hwi0Params.maskSetting = xdc.module("ti.sysbios.interfaces.IHwi").MaskingOption_ALL;
hwi0Params.arg = 0;
Program.global.hwiTimer2 = Hwi.create(40, "&hwiTimer2Fxn", hwi0Params);
because in file tm4c1294ncpd.h:
#define INT_TIMER2B 40 // 16/32-Bit Timer 2B
the hardware interrupt function:
extern "C" void hwiTimer2Fxn(void)
{
TimerIntClear(TIMER2_BASE, TIMER_TIMB_TIMEOUT);
Swi_post(swiTimer2);
}
But I never get the interrupt.
Can you tell me what is wrong with this code?
And like an additional information if I am changing the TIMER_B to TIMER_A and interrupt number to 39 it is working well.
Thanks
Horea