Hi,
I want to interface an asynchronous device with RM48 HDK.
The device has 64 KB of on-chip static memory, 16 data lines, and 16 address lines, address line A0 gives the byte address, A1-A15 give the word address. It can be configured in both the 8-bit and 16-bit modes. In the 16-bit mode, the address line A0 is not used.
I want to interface this device with RM48 HDK such that I am able to access this device in both 8-bit mode and 16-bit modes.
Please tell me how to use EMIF_A[x:0] and EMIF_BA[1:0] of EMIF for this to work.
Regards
Anila