Hello forum, i have run into yet another problem. This time, i would like to know if it is possible to display a real time image of 1-10, where the number "1" is displayed on the LCD and slowly increases to 10 and resets back to 1.
If this is possible, what are the API functions to be called for this to work?
Thanks very much for assisting me,
Cheers on a good day ahead :)