Other Parts Discussed in Thread: HALCOGEN
Hello,
We are using the Hercules RM49L952ZWT board with NHET1 and NHET 2.
On NHET2, we are using 3 pins for pwm all configured identically in HalcoGen. We are using HalCoGen version 4.3.0. When we run a test using the driver and the same function call for all 3 pins, 2 of the pins output the signal correctly and one is inverting the signal. We do not want this signal to be inverted. Is this a hardware limitation? Why is this happening if all 3 pins are configured the same way in HalCoGen on NHET2? I can screenshot the HalCoGen setting and upload the source function for ADC if you need it. Thank you.