This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIVA 1292 adc READ



Dear forum members,
I am using ADC to read current value and convert to temperature.
unsigned long ulTemp_ValueC;
uint32_t ulADC0_Value;
uint32_t TEMP = 0;
void CTI_CONFIG_TEMPSENSOR()
{
    // The ADC0 peripheral must be enabled for use.
    SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
    // Enable sample sequence 3 with a processor signal trigger.
    ADCSequenceConfigure(ADC0_BASE, 3, ADC_TRIGGER_PROCESSOR, 0);
    // Configure step 0 on sequence 3.  Sample the temperature sensor
    // (ADC_CTL_TS) and configure the interrupt flag (ADC_CTL_IE) to be set
    // when the sample is done.  Tell the ADC logic that this is the last
    // conversion on sequence 3 (ADC_CTL_END).
    ADCSequenceStepConfigure(ADC0_BASE, 3, 0, ADC_CTL_TS | ADC_CTL_IE | ADC_CTL_END);
    // Sample sequence 3 enable
    ADCSequenceEnable(ADC0_BASE, 3);
    // Clear the interrupt status flag
    ADCIntClear(ADC0_BASE, 3);
}
unsigned long CTI_READ_TEMPSENSOR(void)
{
// Trigger the ADC conversion
  ADCProcessorTrigger(ADC0_BASE, 3);
// Wait for conversion to be completed.
    while(!ADCIntStatus(ADC0_BASE, 3, false))
    {
    }
    // Read ADC Value.
    ADCSequenceDataGet(ADC0_BASE, 3, &ulADC0_Value);
    //TEMP = (147.5 - ((187.5 × ulADC0_Value) / 4096));
return(TEMP);
}
Any body please can validate my code....I dont have much idea about ADC operation.......
Regards,
Krishnan