Other Parts Discussed in Thread: TM4C129ENCPDT
Hi,
the chip I am suing is TM4C129ENCPDT.
I am trying to use the ADC ports to sample audio signal. Before I connect real audio signal to the pins, I want to make sure the ADC works fine with DC levels. I am using an external 3V as ADC reference
What I found is that the ADC result on the DC level is not stable. I trigger the sampling sequence at 4 times per second and the reading from the ADC would not not stay near at 0, instead it would fluctuate from 0 t0 70.
The same thing happens if I tie the input to 3V. I cannot get steady reading around 4096, the fluctuation is about the same.
I have no experience on this. I know that certain fluctuation is unavoidable, but I am not clear what is normal and what is not normal. 70 looks too high to me. With 70, I am loosing 6-7 bits!
Can anybody help me what I can do to improve this?
Thanks!