We are in the midst of doing a respin to add functionality, fix some board issues and deal with errata.
We have a clarification question on GPIO #10.
The output rise times are specified for a 50pF load. If the outputs are driving a much smaller load can this result in a much faster rise time and cause the latchup? Or is the output drive rate limited or the output otherwise immune from inducing a latchup on itself?
Robert