Other Parts Discussed in Thread: EK-LM3S8962
Community,
I have a project where I want to connect a strain gauge to my Stellaris EK-LM3S8962 board. I intend to attach the gauge to a metal plate which will have forces acting on it. I want to be able to determine forces and deformation of the plate with the strain gauge and output this to the on-board led. I have experience using the on-board peripherals but nothing external. I would need to pass a voltage through one side of the strain gauge and read the voltage output on the other end. I see on the board there are pins with voltages next to them. Are these the only pins that would be able to send the voltage through the gauge? If this is the case, are there specific pins that would be able to read a voltage input as well? I will be using CCS as a development environment. Any help would be appreciated.
Thanks,
David