Other Parts Discussed in Thread: EK-TM4C1294XL
Hello all,
I am using the EK-TM4C1294XL board to develop my project and I am facing a problem when writing on flash. Also, I am using the driverlib and ti-rtos.
I need to persist some data on flash and, on the first load of the program, I write the data direct to the flash but, after this write, the program freezes in the next command, in my case, a simple System_printf. The debug just stops on this command and does not goes forward. I also started a single program just to nake sure I have no other problems in the original project. My new project does almost nothing in the main.
Please, see the attached code below.
#define FLASH_CONFIG_SECTOR 0xC0000
typedef struct {
uint32_t programmed; // The default value for a programmed section is 0x0000ABCD
uint32_t serverIpAddress[4]; // Server IPAddress
uint32_t serverPort; // Server Port
uint32_t localServerPort; // Local server port
uint32_t equipmentId[8]; // Equipment ID
uint32_t serialNumber[14]; // Equipment SerialNumber
uint32_t partNumber[16]; // Equipment PartNumber
uint32_t reserved[467]; // (512 - number of items above)
} RemottaConfig;
int main(void)
{
uint32_t clock;
unsigned int programmed;
RemottaConfig rc;
// Usar 120MHZ de clock
clock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480), 120000000);
/* Call board init functions */
Board_initGeneral();
Board_initGPIO();
programmed = HWREG(FLASH_CONFIG_SECTOR);
if (programmed == 0xFFFFFFFF) {
System_printf("First RUN.\n");
System_flush();
rc.programmed = FLASH_PROGRAMMED;
rc.serverIpAddress[0] = 192;
rc.serverIpAddress[1] = 168;
rc.serverIpAddress[2] = 10;
rc.serverIpAddress[3] = 122;
rc.serverPort = 5000;
rc.localServerPort = 8000;
memset(rc.equipmentId, 0, sizeof(rc.equipmentId));
memset(rc.serialNumber, 0, sizeof(rc.serialNumber));
memset(rc.partNumber, 0, sizeof(rc.partNumber));
memset(rc.reserved, 0, sizeof(rc.reserved));
FlashErase(FLASH_CONFIG_SECTOR);
FlashProgram((uint32_t *)&rc, FLASH_CONFIG_SECTOR, sizeof(RemottaConfig));
}
System_printf("Here is where my code stops\n");
System_flush();
...
After FlashProgram, I see in the MemoryBrowser the data correctly stored in the flash, as expected.
When I remove the code that uses flash, everything goes ok.
What m I doing wrong?
Hi,
Just to trying to do something different, I added the following code before the line: programmed = HWREG(FLASH_CONFIG_SECTOR);
protection = FlashProtectGet(FLASH_CONFIG_SECTOR);
switch(protection) {
case FlashReadWrite:
System_printf("We can read and write on flash");
break;
case FlashReadOnly:
System_printf("Just for reading");
break;
case FlashExecuteOnly:
System_printf("just for executing");
break;
}
System_flush();
And I am receiving the value FlashReadWrite.
Tks in advance.
Leandro