This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem in Coincident sampling mode for both ADC

Hi!
I want to sample both ADC0 and ADC1 module simultaneously, from PE3 (AIN0) and PE2(AIN1) with hardware averaging but after writing the following code only PE2 is and I get same value from both ADC0 and ADC1. Please check where my configuration is wrong,

#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "inc/hw_gpio.h"
#include "inc/hw_adc.h"
#include "driverlib/sysctl.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom_map.h"
#include "driverlib/gpio.h"
#include "driverlib/adc.h"

#ifdef DEBUG
void
__error__(char *pcFilename, unsigned long ulLine)
{
}
#endif


int main(void)
{
unsigned long ulV_ADC_0=0,v=0;
unsigned long ulI_ADC_1=0,i=0;

SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ); // 40MHz

//
// Enable Peripheral Clocks
//
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC1);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);

//
// Enable pin PE2 for ADC AIN1
//
MAP_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_2);

//
// Enable pin PE3 for ADC AIN0
//
MAP_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_3);

SysCtlADCSpeedSet(SYSCTL_ADCSPEED_1MSPS); // Set Speed for both ADC
ADCSequenceDisable(ADC0_BASE|ADC1_BASE, 3);

ADCPhaseDelaySet(ADC0_BASE|ADC1_BASE,ADC_PHASE_0);

ADCSequenceStepConfigure(ADC0_BASE|ADC1_BASE, 3, 0, ADC_CTL_CH0|ADC_CTL_CH1 | ADC_CTL_IE |ADC_CTL_END);

ADCSequenceEnable(ADC0_BASE|ADC1_BASE, 3);

while(1)
{
ADCIntClear(ADC0_BASE|ADC1_BASE, 3);
ADCProcessorTrigger(ADC0_BASE, 3);
while(!ADCIntStatus(ADC0_BASE, 3, false))
{
}
ADCSequenceDataGet(ADC0_BASE, 3, &ulV_ADC_0);
ADCProcessorTrigger(ADC1_BASE, 3);
while(!ADCIntStatus(ADC1_BASE, 3, false))
{
}
ADCSequenceDataGet(ADC1_BASE, 3, &ulI_ADC_1);
v=ulV_ADC_0;
i=ulI_ADC_1;
}
}