This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need some hints about analog input and interrupt generation

Hello,

Could someone give some hints or ideas on how to adress the following issue: 

I want to have an analog input on ADC0 - AIN1 - sequencer 3 (port PF2) and when this input is higher then 1.5 v for example to generate an interrupt (ADC0Seq3_Handler) and n that ISR run some code...

The issue is, it's not clear to me the capabilities of the ADC.
Can the ADC generate an interrupt only when the input value is higher than a certain value? Or should I use the analog comparator? Or digital comparator?

How should the ADC be triggered in this case? By the SW or should run continuesly from startup?

I've been reading the datasheet for TM4c123g and the TivaWare DRL document and unfurtunatly it's still not clear.

Also if you have some examples with a similar situation, it would be great.

Thanks,
Alex

  • Gaal Alexandru said:
    (desired) ... generate an interrupt only when the input value is higher than a certain value? Or should I use the analog comparator? Or digital comparator?   How should the ADC be triggered in this case?

    May we note your (very) complete analysis of the (multiple) options provided by this vendor - that's quite good!

    Now - our experience reveals that each/every method you've listed can be made to work.   Yet my firm has a very strong "favorite" and I bet that we can (successfully) sell that.

    You've identified 3 options - have you not?   Let's list them for clarity:

    • employ the MCU's ADC - this must be programmed to run at a rate sufficient to "catch" your (offending) high-level, analog input signal
    • employ the MCU's analog comparator
    • employ the MCU's digital comparator

    Again all can be made to work - so (which) to choose?   (and why?  i.e. "justify" that choice)

    My firm was (long past) faced w/just this requirement.   (we sought to "kill PWM output" when our BLDC motor controller's "current sensor" detected an "over-current" condition)   This "over-current" condition was noted by our sensor's voltage (exceeding) a known value.   This substantially duplicates your listed conditions - does it not?

     Now you list "no selection criteria" for arriving at your decision.   (consider that)  Ok - time's up - let's (again) list some:

    • reliability/robustness of the chosen effort
    • programming effort required
    • time delay between the arrival of the "offending" signal and the MCU's correcting/preventive response
    • ability of your "method" to be quickly/easily (and dynamically) broadened.   (i.e. you seek to - "on the fly" - alter that 1V5 "trip point.")

    Above list does not insure completeness - yet serves as a reasonable beginning.   Now we must compare/contrast each of these selection criteria against your (earlier) "three identified methods."   And the winner is... ... (hands down - I believe) method #2 "MCU's (on board {chip actually}) Analog Comparator." 

    Now a "blow by blow" justification of the superiority of Analog Comparator:

    • robustness - once the MCU's Analog Comparator is, "Set-Up/Configured" it is substantially "Software error-free" can "protect" even if the MCU lands, "in the weeds."   Your ADC - and especially the ADC's "linked" digital comparator - are "held hostage" to "correctly and continually executing" software - which reduces reliability.
    • program effort - easy victory for MCU's Analog Comparator.   Only "Set-Up" is required - far beyond this is demanded by (other) (i.e. far lesser) methods.
    • time delay (i.e. speed of response to offending input)  Again NO Contest (this is getting boring) Analog Comparator operates at the (always desirable) hardware level - thus proves the "hare" to (outclassed) other method's "tortoise."   (apologies to turtles)  Can your desire (afford) the time delay in responding?   Really?
    • dynamically change your set-point - all other methods demand that you make quite considerable ADC & digital comparator register changes - often in a prescribed manner/order.   Our M4s employ an on-chip DAC - which we feed to the "negative input" of the MCU's Analog Comparator (that's our trip-point input) while the "live input signal is routed to "positive input."   For MCUs (missing) the always helpful DAC - a timer's PWM output can be R-C filtered - serve the same purpose.

    Unstated herein is our treatment of the "MCU's Analog Comparator" output pin.   In our "kill the PWM" application we (simply) route this to the MCU's, "PWM Fault Input" pin - and this level shift proves sufficient to (extinguish) all six PWM outputs.   Yet another benefit - for those offending signals which prove "transient" (i.e. "most of them") - method detailed here (uniquely) provides an "Automatic - Restore to normal operation" capability.   (when the offender "returns to normal" desired operation immediately restores - automatically - which "regulatory agencies" (all) applaud...)

    Has the case in (extremely) strong favor of, "MCU's Analog Comparator" been made to your liking?   We note that it (also) meets your desire for an "example."

  • Sorry, I'm not getting your point.
  • Which point - have you read the entire post? There are (many) points in great support of my recommendation.

    I'm at an airport - net is "in/out" - I compose and "send" in spurts - as connection allows.

    By my (re-read) post is above/beyond (most) here - have you really read slowly/thought/tried to absorb?   How (possibly) can I make (any) clearer?

  • Ok, now I see the full message, just the first two sentences were visible initially.
  • It is (sometimes) unwise to cause your hapless helper to "hang himself" on a national holiday...
  • So... I tried the analog comparator, indeed it's very simple to implement.
    However, I can't figure out how to set the PC6 pin as comparator input.

    The TivaWare file pin_map.h does not contain any macro for the comparator input.

    #define GPIO_PC6_U3RX           0x00021801
    #define GPIO_PC6_PHB1           0x00021806
    #define GPIO_PC6_WT1CCP0        0x00021807
    #define GPIO_PC6_USB0EPEN       0x00021808

    I was expecting something line GPIO_PC6_C0I or C1I... but only comparator outputs are defined for PF0 and PF1 

    #define GPIO_PF0_C0O            0x00050009
    #define GPIO_PF1_C1O            0x00050409

    I assume this might be one of the reasons why I'm not getting any feedback from the comparator ISR.

    My initialization function is the following:

    void COMP_mic_input_init(void)
    {
    	SysCtlPeripheralEnable(SYSCTL_PERIPH_COMP0);		//Comp 0 enable 
    	SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);	 	//Port C enable
    	
    	//GPIOPinConfigure(GPIO_PC6_...);								// ?!?! What to do here :)
    	GPIOPinTypeComparator(GPIO_PORTC_BASE, GPIO_PIN_6);	// Not enaugh???
    	
    	ComparatorConfigure(COMP_BASE,0,COMP_TRIG_NONE|COMP_INT_HIGH|COMP_ASRCP_REF|COMP_OUTPUT_NORMAL);
    	ComparatorRefSet(COMP_BASE,COMP_REF_0_825V);
    	
    	ComparatorIntEnable(COMP_BASE,0);
    }

    And the ISR for the comparator is:

    void Comp0_Handler(void)			//Analog comparator 0 ISR
    {
    	if(ComparatorIntStatus(COMP_BASE,0,false))
    	{
    		ComparatorIntClear(COMP_BASE,0);
    		Motion_Max_Speed();
    	}
    }

  • Hello Gaal,

    Which device are you using?

    Regards
    Amit
  • Hello Gaal,

    Then the following set of lines are sufficient.

    //
    // Enable Peripheral Clocks
    //
    MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);

    //
    // Configure the GPIO Pin Mux for PC7
    // for C0-
    //
    MAP_GPIOPinTypeComparator(GPIO_PORTC_BASE, GPIO_PIN_7);

    //
    // Configure the GPIO Pin Mux for PC6
    // for C0+
    //
    MAP_GPIOPinTypeComparator(GPIO_PORTC_BASE, GPIO_PIN_6);

    Regards
    Amit
  • Why is the "MAP_" index necessary?
    I also added the clock enable for comparator : SysCtlPeripheralEnable(SYSCTL_PERIPH_COMP0);
    Should I delete it?
    Basically I have the same thing in my code as you posted.
  • Hello Gaal

    MAP_ is not required. However the usage of MAP has one important adavantage. If the function has a ROM version, then the application code shall use the ROM version which (a) faster in execution and (b) saves application flash by not having to keep the function in flash.

    Also do check if the startup file have the ISR Mapped and the application code have the call for IntEnable for COMP0 interrupt?

    Regards
    Amit
  • May this reporter note that the (suggested) xx339 (quad comparator) - kicked to the curb - would have been "On the Air" w/in 1 day - Max!

    Ten days have now passed - MCU as "kitchen sink" reveals - again - substantial pain/suffering!    (which was predictable)

    Rejecting the "easy" - for the hard/uncertain - makes sense somewhere & some when. (Yet NOT here - and NOT now!)

  • Hello cb1

    May we note as well, that adding new components, no matter how valuable the advise may be, often creates ripples of doubts.

    Regards
    Amit
  • Hi Amit,

    There's at least one, order of magnitude's EASE, in mastering xx339 vs. MCU's (especially) digital comparators.

    You speak of  "ripples of doubt" - yet the "kitchen sink" - lasting here for TEN Days - far exceeds ripple!   Tsunami, anyone?

    xx339 would have been "On the Air" w/in 1 day - MAX!   (and the pond's surface shines like Glass - ripple free...)

  • The startup file has the ISR mapped, also the interrupts are enabled.
    I have two more edge trigered interrupts on GPIO ports in this SW and they work.
    Maybe I don't understand the basic functionality of the analog comparator, so I tried the next two setups:
    1. C0+ (on PC6) my analog input voltage, internal reference voltage (just bellow 1v)
    2. same as above, just hard wired GND to C0- (on PC7), offcourse enabled also this pin for the comparator. Same as above, internal refference voltage.
    The result is the same, no interrupt is generated.
    Am I missing something ?
  • Hello Gaal,

    Can you please share the simplified project so that it can be checked once more by an independent set of eyes!!!

    Regards
    Amit
  • Sure.
    I also check the TI Pin Mux Utility, there the following two lines of code (among others) is generated for my need:

    MAP_GPIOPinConfigure(GPIO_PC6_C0+);
    MAP_GPIOPinConfigure(GPIO_PC7_C0-);

    The problem is, I can't find the GPIO_PC6_C0+ and GPIO_PC7_C0- macros in the pin_map.h file.
    I will try to manually add the address offset.
  • Droidbot_SW_v6_comparator_test.rar

    I made an archive of it. 
    The project is made in Keil IDE.
    The main and startup files are in the root folder, the rest of the code in modules folder.

    comparator_handler and interrupt_handler are the ones handling the comparator

    The simplified version of the SW:

    Droidbot_SW_v6_comparator_test_simplified.rar

  • Hello Gaal

    I checked the simplified code and I do not see IntEnable(INT_COMP0) in the code.

    Regards
    Amit
  • Thank, yes this ose one of the missing lines :)
    I had the Interrupt master enable, also the port F GPIO interupt enable, but not for the comparator.

    Also after this, I had to modify my input to PC7 (C0-) because initially the PC6 (C0+) continuesly generated interrupts, regardless of input voltage.


    But now it's working fine :)

    Best regards,
    Alex

  • Hello Gaal,

    Glad to hear that it is working fine now.

    Regards
    Amit