Hi, I'm designing with TM4C123GH6PM, my main references design guideline are: datasheet, the schematic of TIVA C launchpad and SPMA059-October 2013.
Likewise many doubts arise me, i need reference voltage for ADC in e 64-pin LQFP package, but in page 24 of SPMA059 say: "The 144-pin LQFP routing example for the VREFA+ and VREFA- nets should be followed for the 100-Pin LQFP package, which is not shown in the table. The 64-pin LQFP package does not have dedicated VREFA+ or VREFA- pins."
But onTable 24-5 on page 1360 of the datasheet, say what the minimum voltage for VDDA is 2.97 V. Is possible to connect a reference voltage of 3.0 V from a REF2030 or REF5030?
In Table 23-2. Signals by Pin Number on page 1330 of datasheet, say for PIN 2: "
The positive supply for the analog circuits (ADC, Analog
Comparators, etc.). These are separated from VDD to minimize
the electrical noise contained on VDD from affecting the analog
functions. VDDA pins must be supplied with a voltage that meets
the specification in Table 24-5 on page 1360, regardless of system
implementation."
If a 3.0 V reference is not possible or not recomended, its possible connect a 3.3 V reference voltage like REF3033 or REF5033?, I need precise ADC conversión for sensor operation and calibration.
Thanks!