This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Generate only one Puls with the PWM-Module

Hello everyone,

I'm working with the EK-TM4C1294XL Launchpad and trying to figure out how to generate only one Puls with the PWM-Module.

My idea was to start the Timer an when it reaches Zero to trigger an Interrupt and in the Interrupt to disable the Timer but it doesn't work.

I hope someone can help me.

Best regards


#include "../src/pwm_gpio_driver.h"

volatile int i=0;
void pwm_gpio_config(void){

	     SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);

	     SysCtlPWMClockSet(SYSCTL_PWMDIV_1);

	     SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM0);

	     SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);

	     GPIOPinConfigure(GPIO_PF1_M0PWM1);		/* PF1 */

	     GPIOPinTypePWM(GPIO_PORTF_BASE , GPIO_PIN_1);	/* PF1 */

	     IntRegister(INT_PWM0_0, PWM0_PF1_Handler);		/* PF1 */
	
	     IntEnable(INT_PWM0_0);			/* PF1 */
	    
	     IntMasterEnable();
	
	     PWMIntEnable(PWM0_BASE, PWM_INT_GEN_0);		/* PF1 */	   
	     
	     PWMGenIntTrigEnable(PWM0_BASE, PWM_GEN_0, PWM_INT_CNT_ZERO );		/* PF1 */
	     
	     PWMGenConfigure(PWM0_BASE,PWM_GEN_0, PWM_GEN_MODE_DOWN | PWM_GEN_MODE_NO_SYNC);	/* PF1 */
	  
	     PWMGenPeriodSet(PWM0_BASE,PWM_GEN_0, Frequency);	/* PF1 */
	     
	     
	     PWMPulseWidthSet(PWM0_BASE,PWM_OUT_1,(1600*Duty_Cycle));	/* PF1 */

	     PWMGenEnable(PWM0_BASE, PWM_GEN_0);	/* PF1 */
	     PWMOutputState(PWM0_BASE, (PWM_OUT_1_BIT), true);
 }

 void PWM0_PF1_Handler(void)
 {
	 /* Clears the specified interrupt for the specified PWM generator block. */
	 PWMGenIntClear(PWM0_BASE, PWM_GEN_0, PWM_INT_CNT_ZERO);

         PWMGenDisable(PWM0_BASE, PWM_GEN_0);

	 /* Disabling the PF1 PWM Output */
	// PWMOutputState(PWM0_BASE, (PWM_OUT_1_BIT), false);
 }