This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123GH6PM PWM clock problem

Hi, i trying to make a simple code to understand more about PWM. Basically, when i press SW1 or SW2, the duty circle change and the brightness of red led change. But when i read the clock of PWM, system and period, the result isn't like i expected

the PWMclock not equa to sysclock/16 = 4mhz/16 = 250000, can some one explain why i got the pwmclock result like that, did i understand any thing wrong?.

Sorry because my crappy english.
Thanks

#include <stdint.h> #include <stdbool.h> #include <math.h> #include <time.h> #include "inc/hw_types.h" #include "inc/hw_memmap.h" #include "driverlib/adc.h" #include "inc/tm4c123gh6pm.h" #include "inc/hw_ssi.h" #include "driverlib/gpio.h" #include "driverlib/fpu.h" #include "driverlib/hibernate.h" #include "driverlib/interrupt.h" #include "driverlib/pin_map.h" #include "driverlib/rom.h" #include "driverlib/sysctl.h" #include "driverlib/systick.h" #include "driverlib/uart.h" #include "driverlib/timer.h" #include "driverlib/ssi.h" #include "inc/hw_ints.h" #include "driverlib/pwm.h" #include "inc/hw_gpio.h" void ButtonISR(void); long ulDutyCycle=50;//Duty cycle of PWM long ulPeriod;//Period of PWM int read; int64_t a,b,c,d; #define LED_RED GPIO_PIN_1 #define LED_BLUE GPIO_PIN_2 #define LED_GREEN GPIO_PIN_3 #define SW1 GPIO_PIN_4 #define SW2 GPIO_PIN_0 void ButtonISR() { GPIOIntClear(GPIO_PORTF_BASE, SW1|SW2); PWMGenDisable(PWM1_BASE, PWM_GEN_2); GPIOPinWrite(GPIO_PORTF_BASE,LED_GREEN|LED_BLUE, LED_GREEN|LED_BLUE); a = PWMGenPeriodGet(PWM1_BASE, PWM_GEN_2); b = PWMPulseWidthGet(PWM1_BASE, PWM_OUT_5); c = SysCtlPWMClockGet(); d = SysCtlClockGet(); read=GPIOPinRead(GPIO_PORTF_BASE,SW1|SW2); if((read&SW1 )==0) { ulDutyCycle = ulDutyCycle+5; } else if((read&SW2)==0) { ulDutyCycle = ulDutyCycle-5; } if(ulDutyCycle>=100) { ulDutyCycle=99; } else if(ulDutyCycle<=0) { ulDutyCycle=1; } //GPIOPinWrite(GPIO_PORTF_BASE,LED_GREEN|LED_BLUE, 0); PWMPulseWidthSet(PWM1_BASE, PWM_OUT_5,ulPeriod*ulDutyCycle/100); PWMGenEnable(PWM1_BASE, PWM_GEN_2); } void main(void) { SysCtlClockSet(SYSCTL_SYSDIV_50|SYSCTL_USE_PLL|SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ); // sys clock = 4mhz SysCtlPWMClockSet(SYSCTL_PWMDIV_16); // pwm clock = 4mhz/16 = 250khz SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF); //Config GPIO that connect to LED - PIN 2,3 //GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE,GPIO_PIN_2|GPIO_PIN_3); //Turn LEDs //GPIOPinWrite(GPIO_PORTF_BASE,LED_GREEN|LED_BLUE, LED_GREEN|LED_BLUE); //Config Buttons HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY; HWREG(GPIO_PORTF_BASE + GPIO_O_CR) |= 0x01; HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = 0; GPIODirModeSet(GPIO_PORTF_BASE, SW1|SW2, GPIO_DIR_MODE_IN); GPIOPadConfigSet(GPIO_PORTF_BASE, SW1|SW2, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU); GPIOIntTypeSet(GPIO_PORTF_BASE,SW1|SW2, GPIO_FALLING_EDGE); GPIOIntRegister(GPIO_PORTF_BASE,&ButtonISR); GPIOIntEnable(GPIO_PORTF_BASE,SW1|SW2); IntEnable(INT_GPIOF); IntMasterEnable(); //Enable the peripherals used by this program. SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM1);// SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF); ulPeriod = (SysCtlPWMClockGet()/250); // //Configure PF1 pins as PWM GPIOPinTypePWM(GPIO_PORTF_BASE, GPIO_PIN_1); GPIOPinConfigure(GPIO_PF1_M1PWM5); //Configure PWM Options PWMGenConfigure(PWM1_BASE, PWM_GEN_2, PWM_GEN_MODE_DOWN); PWMGenPeriodSet(PWM1_BASE, PWM_GEN_2, ulPeriod); // 1s PWMPulseWidthSet(PWM1_BASE, PWM_OUT_5, ulPeriod*ulDutyCycle/100); //Turn on the Output pins PWMOutputState(PWM1_BASE, PWM_OUT_5_BIT, true); //Enable the PWM generator //PWMGenEnable(PWM1_BASE, PWM_GEN_2); while(1) { } }