This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM Flash Program Error Message

Other Parts Discussed in Thread: TM4C129ENCPDT

I am getting an error message "**ERROR**: Problem starting the BOOTP server" when pressing the program button in the LM Flash Programmer - Build 1613 tool.  I am attempting to update the firmware in two TM4C129ENCPDT processors that were designed into a CPU board.  The IP and MAC address are correct in the Configuration folder.  Wireshark was used to monitor the Ethernet and found that there was no communication activity when the program button was activated.  The error message window popped up immediately.  I am able to ping both processors over the Ethernet.  The firewall was disabled in the PC Laptop and administrative rights was given to the LM Flash Programmer tool.  The Laptop OS is Windows 7 64-bit.  The LM Flash Programmer tool was downloaded from the TI website to a different computer and had the same issue.

  

Updates were successfully made to the TM4C129ENCPDT processor on the CPU board by the offsite engineering development team with the identical set up using the LM Flash programmer.  The offsite team did not have any issues when using the Windows 7 or XP operating system.

There must be a software setting(s) in the laptop that is not properly set since the LM Flash programmer has been successfully used with the CPU board previously when connected with a different laptop.

What setting(s) in the Laptop PC is preventing the LM Flash programmer from communicating with the TI processor?

  • Hello Sam,

    Is your PC a Win 7 machine as well? The BOOTP server not starting is a failure of the Socket creation on windows. I would suggest checking why a CreateSocket would fail on Windows with MSDN.

    Regards
    Amit
  • Amit,

    Yes, my laptop is a Windows 7 as well.

    I will look at Socket Creation tomorrow morning.

    Thanks,
    Sam Rummel
    GCMS Engineer
    Advanced Cabin Programs
    Gulfstream Aerospace
    32 Innovation Dr.
    Dept. 499 M/S R-08
    Savannah, GA 31407
    Office: (912) 395-0473


    This e-mail message, including all attachments, is for the sole use of the intended recipient(s) and may contain Personal Information under General Dynamics policy CP 07-105 and/or legally privileged and confidential information.  Any Personal Information can be accessed only by authorized personnel of General Dynamics and its approved service providers and may be used only as permitted by General Dynamics and its policies.  Contractual restrictions apply to third parties.  If you are not an intended recipient, you are hereby notified that you have either received this message in error or through interception, and that any review, use, distribution, copying or disclosure of this message or its attachments is strictly prohibited and is subject to criminal and civil penalties.  All personal messages express solely the sender's views and not those of Gulfstream Aerospace Corporation.
    If you received this message in error, please contact the sender by reply e-mail and destroy all copies of the