This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to Find CGI parameters

Hello !

I trying to modify the enet_io example of Tivaware C Series, I want to send the data from webpage to board via CGI handlers, here is the part of code shown below :

This CGI handler is called whenever the web browser requests iocontrol.cgi.

//

//*****************************************************************************

static char *

ControlCGIHandler(int32_t iIndex, int32_t i32NumParams, char *pcParam[],

char *pcValue[])

{

int32_t i32LEDState, i32Speed;

bool bParamError;

//

// We have not encountered any parameter errors yet.

//

bParamError = false;

//

// Get each of the expected parameters.

//

i32LEDState = FindCGIParameter("LEDOn", pcParam, i32NumParams);

i32Speed = GetCGIParam("speed_percent", pcParam, pcValue, i32NumParams,

&bParamError);

//

// Was there any error reported by the parameter parser?

//

if(bParamError || (i32Speed < 0) || (i32Speed > 100))

{

return(PARAM_ERROR_RESPONSE);

}

//

// We got all the parameters and the values were within the expected ranges

// so go ahead and make the changes.

//

io_set_led((i32LEDState == -1) ? false : true);

io_set_animation_speed(i32Speed);

//

// Send back the default response page.

//

return(DEFAULT_CGI_RESPONSE);

}

int32_t

FindCGIParameter(const char *pcToFind, char *pcParam[], int32_t iNumParams)

{

int32_t iLoop;

//

// Scan through all the parameters in the array.

//

for(iLoop = 0; iLoop < iNumParams; iLoop++)

{

//

// Does the parameter name match the provided string?

//

if(strcmp(pcToFind, pcParam[iLoop]) == 0)

{

//

// We found a match - return the index.

//

return(iLoop);

}

}

//

// If we drop out, the parameter was not found.

//

return(-1);

}

I want to know that how pcparam[] is located, where it will get find, means where the pcparam[] array wil is stored?

 

Regards