Other Parts Discussed in Thread: TM4C1294NCPDT, EK-TM4C1294XL
Hello,
I have been trying to get the bootloader working on the TM4C1294NC9DT controller but failed and I need some help.
1) My first test was creating a CCS project for the flash bootloader in tivaware in the folder called "boot_loader". I have created the project and linked the driver library, USB library to it. the configurations which I set in "bl_config" file was the following:-
//***************************************************************************** // // bl_config.h - The configurable parameters of the boot loader. // // Copyright (c) 2010-2015 Texas Instruments Incorporated. All rights reserved. // Software License Agreement // // Texas Instruments (TI) is supplying this software for use solely and // exclusively on TI's microcontroller products. The software is owned by // TI and/or its suppliers, and is protected under applicable copyright // laws. You may not combine this software with "viral" open-source // software in order to form a larger program. // // THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS. // NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT // NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY // CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL // DAMAGES, FOR ANY REASON WHATSOEVER. // // This is part of revision 2.1.1.71 of the Tiva Firmware Development Package. // //***************************************************************************** #ifndef __BL_CONFIG_H__ #define __BL_CONFIG_H__ //***************************************************************************** // // The following defines are used to configure the operation of the boot // loader. For each define, its interactions with other defines are described. // First is the dependencies (i.e. the defines that must also be defined if it // is defined), next are the exclusives (i.e. the defines that can not be // defined if it is defined), and finally are the requirements (i.e. the // defines that must be defined if it is defined). // // The following defines must be defined in order for the boot loader to // operate: // // One of CAN_ENABLE_UPDATE, ENET_ENABLE_UPDATE, I2C_ENABLE_UPDATE, // SSI_ENABLE_UPDATE, UART_ENABLE_UPDATE, or USB_ENABLE_UPDATE // APP_START_ADDRESS // STACK_SIZE // BUFFER_SIZE // //***************************************************************************** //***************************************************************************** // // The frequency of the crystal used to clock the microcontroller. // // This defines the crystal frequency used by the microcontroller running the // boot loader. If this is unknown at the time of production, then use the // UART_AUTOBAUD feature to properly configure the UART. // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** #define CRYSTAL_FREQ 25000000 //***************************************************************************** // // This enables the boosting of the LDO voltage to 2.75V. For boot loader // configurations that enable the PLL (for example, using the Ethernet port) // on a part that has the PLL errata, this should be enabled. This applies to // revision A2 of Fury-class devices. // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** //#define BOOST_LDO_VOLTAGE //***************************************************************************** // // The starting address of the application. This must be a multiple of 1024 // bytes (making it aligned to a page boundary). A vector table is expected at // this location, and the perceived validity of the vector table (stack located // in SRAM, reset vector located in flash) is used as an indication of the // validity of the application image. // // The flash image of the boot loader must not be larger than this value. // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** #define APP_START_ADDRESS 0x00001000 //***************************************************************************** // // The address at which the application locates its exception vector table. // This must be a multiple of 1KB (making it aligned to a page boundary). // Typically, an application will start with its vector table and this value // will default to APP_START_ADDRESS. This option is provided to cater for // applications which run from external memory which may not be accessible by // the NVIC (the vector table offset register is only 30 bits long). // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** #define VTABLE_START_ADDRESS 0x00001000 //***************************************************************************** // // The size of a single, erasable page in the flash. This must be a power // of 2. The default value of 1KB represents the page size for the internal // flash on all Tiva MCUs and this value should only be overridden if // configuring a boot loader to access external flash devices with a page size // different from this. // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** #define FLASH_PAGE_SIZE 0x00000400 //***************************************************************************** // // The amount of space at the end of flash to reserved. This must be a // multiple of 1024 bytes (making it aligned to a page boundary). This // reserved space is not erased when the application is updated, providing // non-volatile storage that can be used for parameters. // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** //#define FLASH_RSVD_SPACE 0x00000800 //***************************************************************************** // // The number of words of stack space to reserve for the boot loader. // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** #define STACK_SIZE 64 //***************************************************************************** // // The number of words in the data buffer used for receiving packets. This // value must be at least 3. If using autobauding on the UART, this must be at // least 20. The maximum usable value is 65 (larger values will result in // unused space in the buffer). // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** #define BUFFER_SIZE 20 //***************************************************************************** // // Enables updates to the boot loader. Updating the boot loader is an unsafe // operation since it is not fully fault tolerant (losing power to the device // part way though could result in the boot loader no longer being present in // flash). // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** //#define ENABLE_BL_UPDATE //***************************************************************************** // // This definition will cause the the boot loader to erase the entire flash on // updates to the boot loader or to erase the entire application area when the // application is updated. This erases any unused sections in the flash before // the firmware is updated. // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** //#define FLASH_CODE_PROTECTION //***************************************************************************** // // Enables the call to decrypt the downloaded data before writing it into // flash. The decryption routine is empty in the reference boot loader source, // which simply provides a placeholder for adding an actual decrypter. // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** //#define ENABLE_DECRYPTION //***************************************************************************** // // Enables support for the MOSCFAIL handler in the NMI interrupt. // Note: Sandstorm or Fury devices do not provide the MOSCFAIL reset, so this // feature should not be enabled for these devices. // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** //#define ENABLE_MOSCFAIL_HANDLER //***************************************************************************** // // Enables the pin-based forced update check. When enabled, the boot loader // will go into update mode instead of calling the application if a pin is read // at a particular polarity, forcing an update operation. In either case, the // application is still able to return control to the boot loader in order to // start an update. // // Depends on: None // Exclusive of: None // Requires: FORCED_UPDATE_PERIPH, FORCED_UPDATE_PORT, FORCED_UPDATE_PIN, // FORCED_UPDATE_POLARITY // //***************************************************************************** #define ENABLE_UPDATE_CHECK //***************************************************************************** // // The GPIO module to enable in order to check for a forced update. This will // be one of the SYSCTL_RCGCGPIO_Rx values, where Rx represnts the required // GPIO port. This applies to Blizzard class and later devices for FORCED_UPDATE_PORT. // // Depends on: ENABLE_UPDATE_CHECK // Exclusive of: None // Requries: None // //***************************************************************************** #define FORCED_UPDATE_PERIPH SYSCTL_RCGCGPIO_R8 //***************************************************************************** // // The GPIO port to check for a forced update. This will be one of the // GPIO_PORTx_BASE values, where "x" is replaced with the port name (such as // B). The value of "x" should match the value of "x" for // FORCED_UPDATE_PERIPH. // // Depends on: ENABLE_UPDATE_CHECK // Exclusive of: None // Requries: None // //***************************************************************************** #define FORCED_UPDATE_PORT GPIO_PORTJ_BASE //***************************************************************************** // // The pin to check for a forced update. This is a value between 0 and 7. // // Depends on: ENABLE_UPDATE_CHECK // Exclusive of: None // Requries: None // //***************************************************************************** #define FORCED_UPDATE_PIN 0 //***************************************************************************** // // The polarity of the GPIO pin that results in a forced update. This value // should be 0 if the pin should be low and 1 if the pin should be high. // // Depends on: ENABLE_UPDATE_CHECK // Exclusive of: None // Requries: None // //***************************************************************************** #define FORCED_UPDATE_POLARITY 0 //***************************************************************************** // // This enables a weak pull up for the GPIO pin used in a forced update. This // value should be 0 if the pin should be have an internal weak pull down and // 1 if the pin should have an interal weak pull up. // Only FORCED_UPDATE_WPU or FORCED_UPDATE_WPD or neither should be defined. // // Depends on: ENABLE_UPDATE_CHECK // Exclusive of: None // Requries: None // //***************************************************************************** #define FORCED_UPDATE_WPU //#define FORCED_UPDATE_WPD //***************************************************************************** // // This enables the use of the GPIO_LOCK mechanism for configuration of // protected GPIO pins (for example JTAG pins). If this value is not defined, // the locking mechanism will not be used. The only legal values for this // feature are GPIO_LOCK_KEY for Fury devices and GPIO_LOCK_KEY_DD for all // other devices except Sandstorm devices, which do not support this feature. // // Depends on: ENABLE_UPDATE_CHECK // Exclusive of: None // Requries: None // //***************************************************************************** //#define FORCED_UPDATE_KEY GPIO_LOCK_KEY //#define FORCED_UPDATE_KEY GPIO_LOCK_KEY_DD //***************************************************************************** // // Selects the UART as the port for communicating with the boot loader. // // Depends on: None // Exclusive of: CAN_ENABLE_UPDATE, ENET_ENABLE_UPDATE, I2C_ENABLE_UPDATE, // SSI_ENABLE_UPDATE, USB_ENABLE_UPDATE // Requires: UART_AUTOBAUD or UART_FIXED_BAUDRATE // //***************************************************************************** //#define UART_ENABLE_UPDATE //***************************************************************************** // // Enables automatic baud rate detection. This can be used if the crystal // frequency is unknown, or if operation at different baud rates is desired. // // Depends on: UART_ENABLE_UPDATE // Exclusive of: UART_FIXED_BAUDRATE // Requires: None // //***************************************************************************** //#define UART_AUTOBAUD //***************************************************************************** // // Selects the baud rate to be used for the UART. // // Depends on: UART_ENABLE_UPDATE, CRYSTAL_FREQ // Exclusive of: UART_AUTOBAUD // Requires: None // //***************************************************************************** //#define UART_FIXED_BAUDRATE 115200 //***************************************************************************** // // Selects the SSI port as the port for communicating with the boot loader. // // Depends on: None // Exclusive of: CAN_ENABLE_UPDATE, ENET_ENABLE_UPDATE, I2C_ENABLE_UPDATE, // UART_ENABLE_UPDATE, USB_ENABLE_UPDATE // Requires: None // //***************************************************************************** //#define SSI_ENABLE_UPDATE //***************************************************************************** // // Selects the I2C port as the port for communicating with the boot loader. // // Depends on: None // Exclusive of: CAN_ENABLE_UPDATE, ENET_ENABLE_UPDATE, SSI_ENABLE_UPDATE, // UART_ENABLE_UPDATE, USB_ENABLE_UPDATE // Requires: I2C_SLAVE_ADDR // //***************************************************************************** //#define I2C_ENABLE_UPDATE //***************************************************************************** // // Specifies the I2C address of the boot loader. // // Depends on: I2C_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define I2C_SLAVE_ADDR 0x42 //***************************************************************************** // // Selects Ethernet update via the BOOTP/TFTP protocol. // // Depends on: None // Exclusive of: CAN_ENABLE_UPDATE, I2C_ENABLE_UPDATE, SSI_ENABLE_UPDATE, // UART_ENABLE_UPDATE, USB_ENABLE_UPDATE // Requires: CRYSTAL_FREQ // //***************************************************************************** //#define ENET_ENABLE_UPDATE //***************************************************************************** // // Selects if the Ethernet LEDs should be enabled. // // Depends on: ENET_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define ENET_ENABLE_LEDS //***************************************************************************** // // Selects the Ethernet MAC address. If not specified, the MAC address is // taken from the user registers. // // Depends on: ENET_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define ENET_MAC_ADDR0 0x00 //#define ENET_MAC_ADDR1 0x00 //#define ENET_MAC_ADDR2 0x00 //#define ENET_MAC_ADDR3 0x00 //#define ENET_MAC_ADDR4 0x00 //#define ENET_MAC_ADDR5 0x00 //***************************************************************************** // // Sets the name of the BOOTP server to use. This can be used to request that // a particular BOOTP server respond to our request; the value will be either // the server's name, or a nickname used by that server. If not defined then // any BOOTP server is allowed to respond. // // Depends on: ENET_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define ENET_BOOTP_SERVER "tiva" //***************************************************************************** // // Selects USB update via Device Firmware Update class. // // Depends on: None // Exclusive of: CAN_ENABLE_UPDATE, ENET_ENABLE_UPDATE, I2C_ENABLE_UPDATE, // SSI_ENABLE_UPDATE, UART_ENABLE_UPDATE, // Requires: CRYSTAL_FREQ, USB_VENDOR_ID, USB_PRODUCT_ID // //***************************************************************************** #define USB_ENABLE_UPDATE //***************************************************************************** // // The USB vendor ID published by the DFU device. This value is the TI // Tiva vendor ID. Change this to the vendor ID you have been assigned by // USB-IF. // // Depends on: USB_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** #define USB_VENDOR_ID 0x1cbe //***************************************************************************** // // The USB device ID published by the DFU device. If you are using your own // vendor ID, chose a device ID that is different from the ID you use in // non-update operation. If you have sublicensed TI's vendor ID, you must // use an assigned product ID here. // // Depends on: USB_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** #define USB_PRODUCT_ID 0x00ff //***************************************************************************** // // Selects the BCD USB device release number published in the device // descriptor. // // Depends on: USB_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** #define USB_DEVICE_ID 0x0001 //***************************************************************************** // // Sets the maximum power consumption that the DFU device will report to the // USB host in the configuration descriptor. Units are milliamps. // // Depends on: USB_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** #define USB_MAX_POWER 150 //***************************************************************************** // // Determines whether the DFU device reports to the host that it is self // powered (defined as 0) or bus powered (defined as 1). // // Depends on: USB_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** #define USB_BUS_POWERED 1 //***************************************************************************** // // Specifies the GPIO peripheral associated with the USB host/device mux. // // Depends on: USB_ENABLE_UPDATE // Exclusive of: None // Requires: USB_MUX_PERIPH, USB_MUX_PORT, USB_MUX_PIN, USB_MUX_DEVICE // //***************************************************************************** //#define USB_HAS_MUX //***************************************************************************** // // Specifies the GPIO peripheral associated with the USB host/device mux. // // Depends on: USB_ENABLE_UPDATE, USB_HAS_MUX // Exclusive of: None // Requires: None // //***************************************************************************** //#define USB_MUX_PERIPH SYSCTL_RCGC2_GPIOH //***************************************************************************** // // Specifies the GPIO port associated with the USB host/device mux. // // Depends on: USB_ENABLE_UPDATE, USB_HAS_MUX // Exclusive of: None // Requires: None // //***************************************************************************** //#define USB_MUX_PORT GPIO_PORTH_BASE //***************************************************************************** // // Specifies the GPIO pin number used to switch the USB host/device mux. Valid // values are 0 through 7. // // Depends on: USB_ENABLE_UPDATE, USB_HAS_MUX // Exclusive of: None // Requires: None // //***************************************************************************** //#define USB_MUX_PIN 2 //***************************************************************************** // // Specifies the state to set the GPIO pin to to select USB device mode via // the USB host/device mux. Valid values are 1 (high) or 0 (low). // // Depends on: USB_ENABLE_UPDATE, USB_HAS_MUX // Exclusive of: None // Requires: None // //***************************************************************************** //#define USB_MUX_DEVICE 1 //***************************************************************************** // // Selects the CAN port as the port for communicating with the boot loader. // // Depends on: None // Exclusive of: ENET_ENABLE_UPDATE, I2C_ENABLE_UPDATE, SSI_ENABLE_UPDATE, // UART_ENABLE_UPDATE, USB_ENABLE_UPDATE // Requires: CAN_RX_PERIPH, CAN_RX_PORT, CAN_RX_PIN, CAN_TX_PERIPH, // CAN_TX_PORT, CAN_TX_PIN, CAN_BIT_RATE, CRYSTAL_FREQ. // //***************************************************************************** //#define CAN_ENABLE_UPDATE //***************************************************************************** // // Enables the UART to CAN bridging for use when the CAN port is selected for // communicating with the boot loader. // // Depends on: CAN_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define CAN_UART_BRIDGE //***************************************************************************** // // Specifies the GPIO peripheral associated with CAN0 RX pin used by the boot // loader. // // Depends on: CAN_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define CAN_RX_PERIPH SYSCTL_RCGC2_GPIOA //***************************************************************************** // // Specifies the GPIO port associated with CAN0 RX pin used by the boot loader. // // Depends on: CAN_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define CAN_RX_PORT GPIO_PORTA_BASE //***************************************************************************** // // Specifies the GPIO pin number associated with CAN0 RX pin used by the boot // loader. // // Depends on: CAN_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define CAN_RX_PIN 4 //***************************************************************************** // // Specifies the GPIO peripheral associated with CAN0 TX pin used by the boot // loader. // // Depends on: CAN_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define CAN_TX_PERIPH SYSCTL_RCGC2_GPIOA //***************************************************************************** // // Specifies the GPIO port associated with CAN0 TX pin used by the boot loader. // // Depends on: CAN_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define CAN_TX_PORT GPIO_PORTA_BASE //***************************************************************************** // // Specifies the GPIO pin number associated with CAN0 TX pin used by the boot // loader. // // Depends on: CAN_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define CAN_TX_PIN 5 //***************************************************************************** // // Specifies the bit rate for CAN0 used by the boot loader. // // Depends on: CAN_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define CAN_BIT_RATE 1000000 //***************************************************************************** // // Boot loader hook functions. // // The following defines allow you to add application-specific function which // are called at various points during boot loader execution. // //***************************************************************************** //***************************************************************************** // // Performs application-specific low level hardware initialization on system // reset. // // If hooked, this function will be called immediately after the boot loader // code relocation completes. An application may perform any required low // hardware initialization during this function. Note that the system clock // has not been set when this function is called. Initialization that assumes // the system clock is set may be performed in the BL_INIT_FN_HOOK function // instead. // // void MyHwInitFunc(void); // //***************************************************************************** //#define BL_HW_INIT_FN_HOOK MyHwInitFunc //***************************************************************************** // // Performs application-specific initialization on system reset. // // If hooked, this function will be called immediately after the boot loader // sets the system clock. An application may perform any additional // initialization during this function. // // void MyInitFunc(void); // //***************************************************************************** //#define BL_INIT_FN_HOOK MyInitFunc //***************************************************************************** // // Performs application-specific reinitialization on boot loader entry via SVC. // // If hooked, this function will be called immediately after the boot loader // reinitializes the system clock when it is entered from an application // via the SVC mechanism rather than as a result of a system reset. An // application may perform any additional reinitialization in this function. // // void MyReinitFunc(void); // //***************************************************************************** //#define BL_REINIT_FN_HOOK MyReinitFunc //***************************************************************************** // // Informs an application that a download is starting. // // If hooked, this function will be called when a new firmware download is // about to start. The application may use this signal to initialize any // progress display. // // void MyStartFunc(void); // //***************************************************************************** //#define BL_START_FN_HOOK MyStartFunc //***************************************************************************** // // Informs an application of download progress. // // If hooked, this function will be called periodically during firmware // download. The application may use this to update its user interface. // When using a protocol which does not inform the client of the final size of // the download in advance (e.g. TFTP), the ulTotal parameter will be 0, // otherwise it indicates the expected size of the complete download. // // void MyProgressFunc(unsigned long ulCompleted, unsigned long ulTotal); // // where: // // - ulCompleted indicates the number of bytes already downloaded. // - ulTotal indicates the number of bytes expected or 0 if this is not known. // //***************************************************************************** //#define BL_PROGRESS_FN_HOOK MyProgressFunc //***************************************************************************** // // Informs an application that a download has completed. // // If hooked, this function will be called when a firmware download ends. // The application may use this signal to update its user interface. Typically // a system reset will occur shortly after this function returns as the boot // loader attempts to boot the new image. // // void MyEndFunc(void); // //***************************************************************************** //#define BL_END_FN_HOOK MyEndFunc //***************************************************************************** // // Allows an application to perform in-place data decryption during download. // // If hooked, this function will be called on receipt of any new block of // downloaded firmware image data. The application must decrypt this data // in place then return at which point the boot loader will write the data to // flash. // // void MyDecryptionFunc(unsigned char *pucBuffer, unsigned long ulSize); // // where: // // - pucBuffer points to the first byte of data to be decrypted. // - ulSize indicates the number of bytes of data at pucBuffer. // //***************************************************************************** //#define BL_DECRYPT_FN_HOOK MyDecryptionFunc //***************************************************************************** // // Allows an application to force a new firmware download. // // If hooked, this function will be called after a system reset (following // basic initialization and the initialization hook function) to give the // application an opportunity to force a new firmware download. Depending upon // the return code, the boot loader will either boot the existing firmware // image or wait for a new download to be started. // // Note that this hook takes precedence over ENABLE_UPDATE_CHECK settings. If // the hook function is defined, the basic GPIO check offered by // ENABLE_UPDATE_CHECK does not take place. // // unsigned long MyCheckUpdateFunc(void); // // where the return code is 0 if the boot loader should boot the existing // image (if found) or non-zero to indicate that the boot loader should retain // control and wait for a new firmware image to be downloaded. // //***************************************************************************** //#define BL_CHECK_UPDATE_FN_HOOK MyCheckUpdateFunc //***************************************************************************** // // Allows an application to replace the flash block erase function. // // If hooked, this function will be called whenever a block of flash is to // be erased. The function must erase the block and block until the operation // has completed. The size of the block which will be erased is defined by // FLASH_BLOCK_SIZE. // // void MyFlashEraseFunc(unsigned long ulBlockAddr); // // where: // // - ulBlockAddr is the address of the flash block to be erased. // //***************************************************************************** //#define BL_FLASH_ERASE_FN_HOOK MyFlashEraseFunc //***************************************************************************** // // Allows an application to replace the flash programming function. // // If hooked, this function will be called whenever a block of data is to be // be written to flash. The function must program the supplied data and block // until the operation has has completed. // // void MyFlashProgramFunc(unsigned long ulDstAddr, // unsigned char *pucSrcData, // unsigned long ulLength); // // where: // // - ulDstAddr is the address in flash at which the data is to be programmed. // This must be a multiple of 4. // - pucSrcData points to the first byte of the data to program. // - ulLength is the number of bytes of data to program. This must be a // multiple of 4. // //***************************************************************************** //#define BL_FLASH_PROGRAM_FN_HOOK MyFlashProgramFunc //***************************************************************************** // // Allows an application to replace the flash error clear function. // // If hooked, this function will be called before each flash erase or program // operation. The function must clear any flash error indicators and prepare // to detect access violations that may occur in a future erase or program // operation. // // void MyFlashClearErrorFunc(void); // //***************************************************************************** //#define BL_FLASH_CL_ERR_FN_HOOK MyFlashClearErrorFunc //***************************************************************************** // // Reports whether or not a flash access violation error has occurred. // // If hooked, this function will be called after flash erase or program // operations. The return code indicates to the caller whether or not // an access violation error has occurred since the last call to the function // defined by BL_FLASH_CL_ERR_FN_HOOK. // // unsigned long MyFlashErrorFunc(void); // // where the return code is 0 if no error has occurred or non-zero if an // error was detected. // //***************************************************************************** //#define BL_FLASH_ERROR_FN_HOOK MyFlashErrorFunc //***************************************************************************** // // Reports the total size of the device flash. // // If hooked, this function will be called to determine the size of the flash // device. // // unsigned long MyFlashSizeFunc(void); // // where the return code is the total number of bytes of flash supported by the // device. Note that this does not take into account any reserved space // defined via the FLASH_RSVD_SPACE value in this header file. // //***************************************************************************** //#define BL_FLASH_SIZE_FN_HOOK MyFlashSizeFunc //***************************************************************************** // // Reports the address of the first byte after the end of the device flash. // // If hooked, this function will be called to determine the address of the end // of valid flash. // // unsigned long MyFlashEndFunc(void); // // where the return code is the address of the first byte after the end of flash. // Note that this does not take into account any reserved space defined via // the FLASH_RSVD_SPACE value in this header file. // //***************************************************************************** //#define BL_FLASH_END_FN_HOOK MyFlashEndFunc //***************************************************************************** // // Checks whether the start address and size of an image are valid. // // If hooked, this function will be called whenever a new download is to be // started. It determines whether or not an image of a particular size may be // flashed at a given address. Valid addresses are: // // 1. APP_START_ADDRESS in all cases. // 2. 0x00000000 if ENABLE_BL_UPDATE is defined. // 3. The start of the reserved space if FLASH_RSVD_SPACE is defined. // // unsigned long MyFlashAddrCheckFunc(unsigned long ulAddr, // unsigned long ulSize); // // where: // // - ulAddr is the address in flash at which the image is to be programmed. // - ulSize is the total size of the image if known or 0 otherwise. // // The return code will be 0 if the address or size is invalid or a non-zero // value if valid. // //***************************************************************************** //#define BL_FLASH_AD_CHECK_FN_HOOK MyFlashAddrCheckFunc #endif // __BL_CONFIG_H__
I have also commented the whole bl_config.c file since it wasn't compiling. the project was built but with the following log which includes warnings:-
**** Build of configuration Debug__TI for project bootloader ****
"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
'Building file: ../bl_autobaud.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/include" --include_path="F:/ti/TivaWare2.1.1.7" --include_path="F:/ti/TivaWare2.1.1.7/boot_loader" -g --gcc --define=ccs="ccs" --define=TARGET_IS_TM4C129_RA0 --define=UART_BUFFERED --define=PART_TM4C1294NCPDT --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="bl_autobaud.pp" "../bl_autobaud.c"
'Finished building: ../bl_autobaud.c'
' '
'Building file: ../bl_can.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/include" --include_path="F:/ti/TivaWare2.1.1.7" --include_path="F:/ti/TivaWare2.1.1.7/boot_loader" -g --gcc --define=ccs="ccs" --define=TARGET_IS_TM4C129_RA0 --define=UART_BUFFERED --define=PART_TM4C1294NCPDT --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="bl_can.pp" "../bl_can.c"
'Finished building: ../bl_can.c'
' '
'Building file: ../bl_check.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/include" --include_path="F:/ti/TivaWare2.1.1.7" --include_path="F:/ti/TivaWare2.1.1.7/boot_loader" -g --gcc --define=ccs="ccs" --define=TARGET_IS_TM4C129_RA0 --define=UART_BUFFERED --define=PART_TM4C1294NCPDT --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="bl_check.pp" "../bl_check.c"
'Finished building: ../bl_check.c'
' '
'Building file: ../bl_config.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/include" --include_path="F:/ti/TivaWare2.1.1.7" --include_path="F:/ti/TivaWare2.1.1.7/boot_loader" -g --gcc --define=ccs="ccs" --define=TARGET_IS_TM4C129_RA0 --define=UART_BUFFERED --define=PART_TM4C1294NCPDT --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="bl_config.pp" "../bl_config.c"
"../bl_config.c", line 48: warning #9-D: nested comment is not allowed
"../bl_config.c", line 52: warning #9-D: nested comment is not allowed
"../bl_config.c", line 55: warning #9-D: nested comment is not allowed
"../bl_config.c", line 59: warning #9-D: nested comment is not allowed
"../bl_config.c", line 62: warning #9-D: nested comment is not allowed
"../bl_config.c", line 66: warning #9-D: nested comment is not allowed
"../bl_config.c", line 71: warning #9-D: nested comment is not allowed
"../bl_config.c", line 75: warning #9-D: nested comment is not allowed
"../bl_config.c", line 80: warning #9-D: nested comment is not allowed
"../bl_config.c", line 84: warning #9-D: nested comment is not allowed
"../bl_config.c", line 89: warning #9-D: nested comment is not allowed
"../bl_config.c", line 93: warning #9-D: nested comment is not allowed
"../bl_config.c", line 98: warning #9-D: nested comment is not allowed
"../bl_config.c", line 102: warning #9-D: nested comment is not allowed
"../bl_config.c", line 107: warning #9-D: nested comment is not allowed
"../bl_config.c", line 111: warning #9-D: nested comment is not allowed
"../bl_config.c", line 116: warning #9-D: nested comment is not allowed
"../bl_config.c", line 120: warning #9-D: nested comment is not allowed
"../bl_config.c", line 130: warning #9-D: nested comment is not allowed
"../bl_config.c", line 134: warning #9-D: nested comment is not allowed
"../bl_config.c", line 144: warning #9-D: nested comment is not allowed
"../bl_config.c", line 148: warning #9-D: nested comment is not allowed
"../bl_config.c", line 158: warning #9-D: nested comment is not allowed
"../bl_config.c", line 163: warning #9-D: nested comment is not allowed
'Finished building: ../bl_config.c'
' '
'Building file: ../bl_crc32.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/include" --include_path="F:/ti/TivaWare2.1.1.7" --include_path="F:/ti/TivaWare2.1.1.7/boot_loader" -g --gcc --define=ccs="ccs" --define=TARGET_IS_TM4C129_RA0 --define=UART_BUFFERED --define=PART_TM4C1294NCPDT --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="bl_crc32.pp" "../bl_crc32.c"
'Finished building: ../bl_crc32.c'
' '
'Building file: ../bl_decrypt.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/include" --include_path="F:/ti/TivaWare2.1.1.7" --include_path="F:/ti/TivaWare2.1.1.7/boot_loader" -g --gcc --define=ccs="ccs" --define=TARGET_IS_TM4C129_RA0 --define=UART_BUFFERED --define=PART_TM4C1294NCPDT --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="bl_decrypt.pp" "../bl_decrypt.c"
'Finished building: ../bl_decrypt.c'
' '
'Building file: ../bl_emac.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/include" --include_path="F:/ti/TivaWare2.1.1.7" --include_path="F:/ti/TivaWare2.1.1.7/boot_loader" -g --gcc --define=ccs="ccs" --define=TARGET_IS_TM4C129_RA0 --define=UART_BUFFERED --define=PART_TM4C1294NCPDT --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="bl_emac.pp" "../bl_emac.c"
'Finished building: ../bl_emac.c'
' '
'Building file: ../bl_flash.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/include" --include_path="F:/ti/TivaWare2.1.1.7" --include_path="F:/ti/TivaWare2.1.1.7/boot_loader" -g --gcc --define=ccs="ccs" --define=TARGET_IS_TM4C129_RA0 --define=UART_BUFFERED --define=PART_TM4C1294NCPDT --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="bl_flash.pp" "../bl_flash.c"
'Finished building: ../bl_flash.c'
' '
'Building file: ../bl_i2c.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/include" --include_path="F:/ti/TivaWare2.1.1.7" --include_path="F:/ti/TivaWare2.1.1.7/boot_loader" -g --gcc --define=ccs="ccs" --define=TARGET_IS_TM4C129_RA0 --define=UART_BUFFERED --define=PART_TM4C1294NCPDT --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="bl_i2c.pp" "../bl_i2c.c"
'Finished building: ../bl_i2c.c'
' '
'Building file: ../bl_main.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/include" --include_path="F:/ti/TivaWare2.1.1.7" --include_path="F:/ti/TivaWare2.1.1.7/boot_loader" -g --gcc --define=ccs="ccs" --define=TARGET_IS_TM4C129_RA0 --define=UART_BUFFERED --define=PART_TM4C1294NCPDT --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="bl_main.pp" "../bl_main.c"
'Finished building: ../bl_main.c'
' '
'Building file: ../bl_packet.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/include" --include_path="F:/ti/TivaWare2.1.1.7" --include_path="F:/ti/TivaWare2.1.1.7/boot_loader" -g --gcc --define=ccs="ccs" --define=TARGET_IS_TM4C129_RA0 --define=UART_BUFFERED --define=PART_TM4C1294NCPDT --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="bl_packet.pp" "../bl_packet.c"
'Finished building: ../bl_packet.c'
' '
'Building file: ../bl_ssi.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/include" --include_path="F:/ti/TivaWare2.1.1.7" --include_path="F:/ti/TivaWare2.1.1.7/boot_loader" -g --gcc --define=ccs="ccs" --define=TARGET_IS_TM4C129_RA0 --define=UART_BUFFERED --define=PART_TM4C1294NCPDT --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="bl_ssi.pp" "../bl_ssi.c"
'Finished building: ../bl_ssi.c'
' '
'Building file: ../bl_startup_ccs.s'
'Invoking: ARM Compiler'
"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/include" --include_path="F:/ti/TivaWare2.1.1.7" --include_path="F:/ti/TivaWare2.1.1.7/boot_loader" -g --gcc --define=ccs="ccs" --define=TARGET_IS_TM4C129_RA0 --define=UART_BUFFERED --define=PART_TM4C1294NCPDT --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="bl_startup_ccs.pp" "../bl_startup_ccs.s"
'Finished building: ../bl_startup_ccs.s'
' '
'Building file: ../bl_uart.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/include" --include_path="F:/ti/TivaWare2.1.1.7" --include_path="F:/ti/TivaWare2.1.1.7/boot_loader" -g --gcc --define=ccs="ccs" --define=TARGET_IS_TM4C129_RA0 --define=UART_BUFFERED --define=PART_TM4C1294NCPDT --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="bl_uart.pp" "../bl_uart.c"
'Finished building: ../bl_uart.c'
' '
'Building file: ../bl_usb.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/include" --include_path="F:/ti/TivaWare2.1.1.7" --include_path="F:/ti/TivaWare2.1.1.7/boot_loader" -g --gcc --define=ccs="ccs" --define=TARGET_IS_TM4C129_RA0 --define=UART_BUFFERED --define=PART_TM4C1294NCPDT --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="bl_usb.pp" "../bl_usb.c"
'Finished building: ../bl_usb.c'
' '
'Building file: ../bl_usbfuncs.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/include" --include_path="F:/ti/TivaWare2.1.1.7" --include_path="F:/ti/TivaWare2.1.1.7/boot_loader" -g --gcc --define=ccs="ccs" --define=TARGET_IS_TM4C129_RA0 --define=UART_BUFFERED --define=PART_TM4C1294NCPDT --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="bl_usbfuncs.pp" "../bl_usbfuncs.c"
'Finished building: ../bl_usbfuncs.c'
' '
'Building target: bootloader.out'
'Invoking: ARM Linker'
"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me -g --gcc --define=ccs="ccs" --define=TARGET_IS_TM4C129_RA0 --define=UART_BUFFERED --define=PART_TM4C1294NCPDT --diag_warning=225 --display_error_number --diag_wrap=off -z -m"bootloader.map" --heap_size=0 --stack_size=512 -i"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/lib" -i"F:/ti/TivaWare2.1.1.7" -i"F:/ti/TivaWare2.1.1.7/boot_loader" -i"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/include" --reread_libs --warn_sections --diag_wrap=off --display_error_number --xml_link_info="bootloader_linkInfo.xml" --rom_model -o "bootloader.out" "./bl_autobaud.obj" "./bl_can.obj" "./bl_check.obj" "./bl_config.obj" "./bl_crc32.obj" "./bl_decrypt.obj" "./bl_emac.obj" "./bl_flash.obj" "./bl_i2c.obj" "./bl_main.obj" "./bl_packet.obj" "./bl_ssi.obj" "./bl_startup_ccs.obj" "./bl_uart.obj" "./bl_usb.obj" "./bl_usbfuncs.obj" "../bl_link_ccs.cmd" -l"libc.a" -l"F:\ti\TivaWare2.1.1.7\driverlib\ccs\Debug\driverlib.lib" -l"F:\ti\TivaWare2.1.1.7\sensorlib\ccs\Debug\sensorlib.lib" -l"F:\ti\TivaWare2.1.1.7\usblib\ccs\Debug\usblib.lib"
<Linking>
warning #10278-D: LOAD placement specified for section ".text:decompress:none:rtsv7M4_T_le_v4SPD16_eabi.lib<copy_decompress_none.obj>". This section contains decompression routines required for linker generated copy tables and C/C++ auto-initialization. Must ensure that this section is copied to run address before the C/C++ boot code is executed or is placed with single allocation specifier (ex. "> MEMORY").
warning #10278-D: LOAD placement specified for section ".text:rtsv7M4_T_le_v4SPD16_eabi.lib<memcpy_t2.obj>". This section contains decompression routines required for linker generated copy tables and C/C++ auto-initialization. Must ensure that this section is copied to run address before the C/C++ boot code is executed or is placed with single allocation specifier (ex. "> MEMORY").
warning #10278-D: LOAD placement specified for section ".text:decompress:ZI:rtsv7M4_T_le_v4SPD16_eabi.lib<copy_zero_init.obj>". This section contains decompression routines required for linker generated copy tables and C/C++ auto-initialization. Must ensure that this section is copied to run address before the C/C++ boot code is executed or is placed with single allocation specifier (ex. "> MEMORY").
warning #10278-D: LOAD placement specified for section ".text:rtsv7M4_T_le_v4SPD16_eabi.lib<memset_t2.obj>". This section contains decompression routines required for linker generated copy tables and C/C++ auto-initialization. Must ensure that this section is copied to run address before the C/C++ boot code is executed or is placed with single allocation specifier (ex. "> MEMORY").
warning #10278-D: LOAD placement specified for section ".text:decompress:rle24:rtsv7M4_T_le_v4SPD16_eabi.lib<copy_decompress_rle.obj>". This section contains decompression routines required for linker generated copy tables and C/C++ auto-initialization. Must ensure that this section is copied to run address before the C/C++ boot code is executed or is placed with single allocation specifier (ex. "> MEMORY").
warning #10278-D: LOAD placement specified for section ".text:rtsv7M4_T_le_v4SPD16_eabi.lib<copy_decompress_rle.obj>". This section contains decompression routines required for linker generated copy tables and C/C++ auto-initialization. Must ensure that this section is copied to run address before the C/C++ boot code is executed or is placed with single allocation specifier (ex. "> MEMORY").
warning #10278-D: LOAD placement specified for section ".text:rtsv7M4_T_le_v4SPD16_eabi.lib<memset_t2.obj>". This section contains decompression routines required for linker generated copy tables and C/C++ auto-initialization. Must ensure that this section is copied to run address before the C/C++ boot code is executed or is placed with single allocation specifier (ex. "> MEMORY").
warning #10247-D: creating output section ".cinit" without a SECTIONS specification
'Finished building target: bootloader.out'
' '
**** Build Finished ****
after flashing, I opened the LM flash programmer tool, connected the USB port from my TM4C1294 launchpad to the PC. But the PC didn't even recognize that there is any device connected to it. which means that the USB protocol is not working at all and I don't know why.
I have also tried selecting UART bootloader from the config file, choose UART in LM flash tool, connecting the launchpad debug port and flashing but it didn't work as well.
2) My second test was creating a simple program to call the ROM UART bootloader and then connecting LM flash programmer to the launchpad debug USB and test, but it failed as well.
Here is my code:-
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_memmap.h"
#include "inc/hw_nvic.h"
#include "inc/hw_types.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "drivers/pinout.h"
uint32_t ui32SysClock;
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, unsigned long ulLine)
{
}
#endif
//*****************************************************************************
//
// A simple application demonstrating use of the boot loader,
//
//*****************************************************************************
int
main(void)
{
//
// Run from the PLL at 120 MHz.
//
ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN | SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
//
// Configure the device pins.
//
// Configure the device pins for this board.
//
PinoutSet(false, false);
//
// Enable the UART that will be used for the firmware update.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
//
// Configure the UART for 115200, 8-N-1.
//
ROM_UARTConfigSetExpClk(UART0_BASE, ui32SysClock, 115200,
(UART_CONFIG_PAR_NONE | UART_CONFIG_STOP_ONE |
UART_CONFIG_WLEN_8));
//
// Enable the UART operation.
//
ROM_UARTEnable(UART0_BASE);
//
// Disable all processor interrupts. Instead of disabling them one at a
// time, a direct write to NVIC is done to disable all peripheral
// interrupts.
//
HWREG(NVIC_DIS0) = 0xffffffff;
HWREG(NVIC_DIS1) = 0xffffffff;
HWREG(NVIC_DIS2) = 0xffffffff;
HWREG(NVIC_DIS3) = 0xffffffff;
HWREG(NVIC_DIS4) = 0xffffffff;
//
// Call the ROM UART boot loader.
//
ROM_UpdateUART();
//
// The boot loader should not return. In the off chance that it does,
// enter a dead loop.
//
while(1)
{
}
}
I know that the MCU UART0 pins are connected to the debugger, so I'm connecting the debugger USB port on the launchpad to the PC and trying to flash in UART mode using the LM flash programmer but I always fail.
I prefer if I can be able to get the USB DFU boorloader working please. any help will be much appreciated.
Thank you,
Ahmed