This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with GPIO (P2) interrupt



Hi there,

I tried to use GPIO (P2) interrupt on TM4C1294. Codes are done on CCS

  1. Interrupt handler is added to startup_ccs.c's GPIO Port P2 entry
  2. MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOP) is called
  3. MAP_GPIOPinTypeGPIOInput(GPIO_PORTP_BASE, GPIO_PIN_2) is called
  4. IntPrioritySet(INT_GPIOP2, 0xc0);
  5. IntEnable(INT_GPIOP2) and IntMasterEnable() are invoked
  6. Applied to P2 is pulses with width of 50us , frequency 64Khz.

but no interrupt is generated, I got a feeling I might need to specify edge/level(?), but I can't find enough info on how to use it, but at this point, I got no interrupt.

What did I missed here?

Thanks for any pointer/reading!