This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

regarding CAN.

Sir,

On reception i am going to set up a message buffer to receive my messages. Now i have to analyse the message that  is check the message ID and see the different cases available and then transmit a message again.Is there any coding for this purpose ? 

Thanks,

Monica

  • Hello Monica,

    You can review the existing CAN exampls in TivaWare D:\ti\TivaWare_C_Series-2.1.1.71\examples\peripherals\can to see how you want to process the message ID's/

    Regards
    Amit
  • Hi Amit,

    May I suggest that poster will especially benefit from the mating program pair, "simple_can_rx.c & simple_can_tx.c."

    My small group - along w/multiple clients - have started w/this pair and rate them highly as an, "early path to CAN mastery."

    Ciao,

  • Hello cb1

    Yes, that is correct. The simple RX and TX code for CAN must be used. I am trying to see if they can be done on a single device with external CAN transceiver to simplify the code.

    Regards
    Amit
  • hello Amit,

    Thank you.
  • Hello Monica

    Note, that in to meet your requirement the application loop must be setup to parse the new message or a Call back function added to handle the message from the interrupt handler with a Software Lock to prevent a new message from corrupting the message under processing in case there are back 2 back messages.

    Regards
    Amit
  • Hello amit,
    I dint understand the use of while being used in the program.
    while(!g_msgobject)
    {
    }
    when the  third message is  sent an interrupt is generated so the  main loop uses it and loads it with fourth message .so what does "while" do here?. when i comment it, the transmission is happening in the right manner. Else there is a problem with the transmission of 4th message using message object 3. 
    Regards,
    Monica G V

  • Hello amit,

    I want to use 3 message objects to send three messages with unique ID's. So i have commented out the fourth ID tCanMsgObject structure inside main loop and also setting the flag in the interrupt handler which is used in main loop. Yet the message is transmited. And we hacve already given the data so the CAN frame will be automatically built or do we have to create that ?
  • Hello Monica,

    Can you please attach the updated code, so that we can see which part is commented and which is not?

    Regards
    Amit
  • //*****************************************************************************
    //
    // multi_tx.c - Peripheral example demonstrating multiple CAN message
    //              transmission.
    //
    // Copyright (c) 2010-2015 Texas Instruments Incorporated.  All rights reserved.
    // Software License Agreement
    // 
    //   Redistribution and use in source and binary forms, with or without
    //   modification, are permitted provided that the following conditions
    //   are met:
    // 
    //   Redistributions of source code must retain the above copyright
    //   notice, this list of conditions and the following disclaimer.
    // 
    //   Redistributions in binary form must reproduce the above copyright
    //   notice, this list of conditions and the following disclaimer in the
    //   documentation and/or other materials provided with the  
    //   distribution.
    // 
    //   Neither the name of Texas Instruments Incorporated nor the names of
    //   its contributors may be used to endorse or promote products derived
    //   from this software without specific prior written permission.
    // 
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // 
    // This is part of revision 2.1.1.71 of the Tiva Firmware Development Package.
    //
    //*****************************************************************************
    
    #include <stdbool.h>
    #include <stdint.h>
    #include "inc/hw_can.h"
    #include "inc/hw_ints.h"
    #include "inc/hw_memmap.h"
    #include "driverlib/can.h"
    #include "driverlib/gpio.h"
    #include "driverlib/interrupt.h"
    #include "driverlib/pin_map.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/uart.h"
    #include "utils/uartstdio.h"
    
    //*****************************************************************************
    //
    //! \addtogroup can_examples_list
    //! <h1>Multiple CAN TX (multi_tx)</h1>
    //!
    //! This example shows how to set up the CAN to send multiple messages.  The
    //! CAN peripheral is configured to send messages with 4 different CAN IDs.
    //! Two of the messages (with different CAN IDs) are sent using a shared
    //! message object.  This shows how to reuse a message object for multiple
    //! messages.  The other two messages are sent using their own message objects.
    //! All four messages are transmitted once per second.  The content of each
    //! message is a test pattern.  A CAN interrupt handler is used to confirm
    //! message transmission and count the number of messages that have been sent.
    //!
    //! This example uses the following peripherals and I/O signals.  You must
    //! review these and change as needed for your own board:
    //! - CAN0 peripheral
    //! - GPIO Port B peripheral (for CAN0 pins)
    //! - CAN0RX - PB4
    //! - CAN0TX - PB5
    //!
    //! The following UART signals are configured only for displaying console
    //! messages for this example.  These are not required for operation of CAN.
    //! - GPIO port A peripheral (for UART0 pins)
    //! - UART0RX - PA0
    //! - UART0TX - PA1
    //!
    //! This example uses the following interrupt handlers.  To use this example
    //! in your own application you must add these interrupt handlers to your
    //! vector table.
    //! - INT_CAN0 - CANIntHandler
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // A counter that keeps track of the number of times the TX interrupt has
    // occurred, which should match the number of TX messages that were sent.
    //
    //*****************************************************************************
    volatile uint32_t g_ui32IntCount = 0;
    
    //*****************************************************************************
    //
    // Counters that are used to count the number of messages on each of the
    // three message objects that are used in this example.
    //
    //*****************************************************************************
    volatile uint32_t g_ui32Msg1Count = 0;
    volatile uint32_t g_ui32Msg2Count = 0;
    volatile uint32_t g_ui32Msg3Count = 0;
    
    //*****************************************************************************
    //
    // A flag to indicate that CAN controller message object 3 has sent a message.
    //
    //*****************************************************************************
    volatile bool g_bMsgObj3Sent = 0;
    
    //*****************************************************************************
    //
    // A flag to indicate that some transmission error occurred.
    //
    //*****************************************************************************
    volatile bool g_bErrFlag = 0;
    
    //*****************************************************************************
    //
    // CAN message objects that will hold the separate CAN messages.  These could
    // also be allocated on the stack but be careful because these structures
    // each take about 20 bytes.
    //
    //*****************************************************************************
    tCANMsgObject g_sCANMsgObject1;
    tCANMsgObject g_sCANMsgObject2;
    tCANMsgObject g_sCANMsgObject3;
    
    //*****************************************************************************
    //
    // Message buffers that hold the contents of the 4 different messages that
    // are being transmitted.  Each one is a different length.
    //
    //*****************************************************************************
    uint8_t g_pui8Msg1[4] = { 0, 0, 0, 0 };
    uint8_t g_pui8Msg2[5] = { 2, 2, 2, 2, 2 };
    uint8_t g_pui8Msg3[6] = { 3, 3, 3, 3, 3, 3 };
    uint8_t g_pui8Msg4[8] = { 4, 4, 4, 4, 5, 5, 5, 5 };
    
    //*****************************************************************************
    //
    // This function sets up UART0 to be used for a console to display information
    // as the example is running.
    //
    //*****************************************************************************
    void
    InitConsole(void)
    {
        //
        // Enable GPIO port A which is used for UART0 pins.
        // TODO: change this to whichever GPIO port you are using.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
    
        //
        // Configure the pin muxing for UART0 functions on port A0 and A1.
        // This step is not necessary if your part does not support pin muxing.
        // TODO: change this to select the port/pin you are using.
        //
        GPIOPinConfigure(GPIO_PA0_U0RX);
        GPIOPinConfigure(GPIO_PA1_U0TX);
    
        //
        // Enable UART0 so that we can configure the clock.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
    
        //
        // Use the internal 16MHz oscillator as the UART clock source.
        //
        UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
    
        //
        // Select the alternate (UART) function for these pins.
        // TODO: change this to select the port/pin you are using.
        //
        GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
    
        //
        // Initialize the UART for console I/O.
        //
        UARTStdioConfig(0, 115200, 16000000);
    }
    
    //*****************************************************************************
    //
    // This function prints some information about the CAN message to the
    // serial port for information purposes only.
    //
    //*****************************************************************************
    void
    PrintCANMessageInfo(tCANMsgObject *psCANMsg, uint32_t ui32MsgObj)
    {
        unsigned int uIdx;
    
        UARTprintf("Sending msg: obj=%d ID=0x%04X msg=0x", ui32MsgObj,
                   psCANMsg->ui32MsgID);
        for(uIdx = 0; uIdx < psCANMsg->ui32MsgLen; uIdx++)
        {
            UARTprintf("%02X ", psCANMsg->pui8MsgData[uIdx]);
        }
        UARTprintf("\n");
    }
    
    //*****************************************************************************
    //
    // This function provides a 1 second delay using a simple polling method.
    //
    //*****************************************************************************
    void
    SimpleDelay(void)
    {
        //
        // Delay cycles for 1 second
        //
        SysCtlDelay(16000000 / 3);
    }
    
    //*****************************************************************************
    //
    // This function is the interrupt handler for the CAN peripheral.  It checks
    // for the cause of the interrupt, and maintains a count of all messages that
    // have been transmitted.
    //
    //*****************************************************************************
    void
    CANIntHandler(void)
    {
        uint32_t ui32Status;
    
        //
        // Read the CAN interrupt status to find the cause of the interrupt
        //
        ui32Status = CANIntStatus(CAN0_BASE, CAN_INT_STS_CAUSE);
    
        //
        // If the cause is a controller status interrupt, then get the status
        //
        if(ui32Status == CAN_INT_INTID_STATUS)
        {
            //
            // Read the controller status.  This will return a field of status
            // error bits that can indicate various errors.  Error processing
            // is not done in this example for simplicity.  Refer to the
            // API documentation for details about the error status bits.
            // The act of reading this status will clear the interrupt.  If the
            // CAN peripheral is not connected to a CAN bus with other CAN devices
            // present, then errors will occur and will be indicated in the
            // controller status.
            //
            ui32Status = CANStatusGet(CAN0_BASE, CAN_STS_CONTROL);
    
            //
            // Set a flag to indicate some errors may have occurred.
            //
            g_bErrFlag = 1;
        }
    
        //
        // Check if the cause is message object 1, which is used for sending
        // message 1.
        //
        else if(ui32Status == 1)
        {
            //
            // Getting to this point means that the TX interrupt occurred on
            // message object 1, and the message TX is complete.  Clear the
            // message object interrupt.
            //
            CANIntClear(CAN0_BASE, 1);
    
            //
            // Increment a counter to keep track of how many messages have been
            // sent.  In a real application this could be used to set flags to
            // indicate when a message is sent.
            //
            g_ui32Msg1Count++;
    
            //
            // Since the message was sent, clear any error flags.
            //
            g_bErrFlag = 0;
        }
    
        //
        // Check if the cause is message object 2, which is used for sending
        // message 2.
        //
        else if(ui32Status == 2)
        {
            //
            // Getting to this point means that the TX interrupt occurred on
            // message object 2, and the message TX is complete.  Clear the
            // message object interrupt.
            //
            CANIntClear(CAN0_BASE, 2);
    
            //
            // Increment a counter to keep track of how many messages have been
            // sent.  In a real application this could be used to set flags to
            // indicate when a message is sent.
            //
            g_ui32Msg2Count++;
    
            //
            // Since the message was sent, clear any error flags.
            //
            g_bErrFlag = 0;
        }
    
        //
        // Check if the cause is message object 3, which is used for sending
        // messages 3 and 4.
        //
        else if(ui32Status == 3)
        {
            //
            // Getting to this point means that the TX interrupt occurred on
            // message object 3, and a message TX is complete.  Clear the
            // message object interrupt.
            //
            CANIntClear(CAN0_BASE, 3);
    
            //
            // Increment a counter to keep track of how many messages have been
            // sent.  In a real application this could be used to set flags to
            // indicate when a message is sent.
            //
            g_ui32Msg3Count++;
    
            //
            // Set the flag indicating that a message was sent using message
            // object 3.  The program main loop uses this to know when to send
            // another message using message object 3.
            //
            g_bMsgObj3Sent = 1;
    
            //
            // Since the message was sent, clear any error flags.
            //
            g_bErrFlag = 0;
        }
    
        //
        // Otherwise, something unexpected caused the interrupt.  This should
        // never happen.
        //
        else
        {
            //
            // Spurious interrupt handling can go here.
            //
        }
    }
    
    //*****************************************************************************
    //
    // Configure the CAN and enter a loop to transmit periodic CAN messages.
    //
    //*****************************************************************************
    int
    main(void)
    {
    #if defined(TARGET_IS_TM4C129_RA0) ||                                         \
    	defined(TARGET_IS_TM4C129_RA1) ||                                         \
        defined(TARGET_IS_TM4C129_RA2)
    	uint32_t ui32SysClock;
    #endif
    
        //
        // Set the clocking to run directly from the external crystal/oscillator.
        // TODO: The SYSCTL_XTAL_ value must be changed to match the value of the
        // crystal on your board.
        //
    #if defined(TARGET_IS_TM4C129_RA0) ||                                         \
    	defined(TARGET_IS_TM4C129_RA1) ||                                         \
        defined(TARGET_IS_TM4C129_RA2)
        ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
                                           SYSCTL_OSC_MAIN |
                                           SYSCTL_USE_OSC)
                                           25000000);
    #else
        SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
                       SYSCTL_XTAL_16MHZ);
    #endif
    
        //
        // Set up the serial console to use for displaying messages.  This is
        // just for this example program and is not needed for CAN operation.
        //
        InitConsole();
    
        //
        // For this example CAN0 is used with RX and TX pins on port B4 and B5.
        // The actual port and pins used may be different on your part, consult
        // the data sheet for more information.
        // GPIO port B needs to be enabled so these pins can be used.
        // TODO: change this to whichever GPIO port you are using
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
    
        //
        // Configure the GPIO pin muxing to select CAN0 functions for these pins.
        // This step selects which alternate function is available for these pins.
        // This is necessary if your part supports GPIO pin function muxing.
        // Consult the data sheet to see which functions are allocated per pin.
        // TODO: change this to select the port/pin you are using
        //
        GPIOPinConfigure(GPIO_PB4_CAN0RX);
        GPIOPinConfigure(GPIO_PB5_CAN0TX);
    
        //
        // Enable the alternate function on the GPIO pins.  The above step selects
        // which alternate function is available.  This step actually enables the
        // alternate function instead of GPIO for these pins.
        // TODO: change this to match the port/pin you are using
        //
        GPIOPinTypeCAN(GPIO_PORTB_BASE, GPIO_PIN_4 | GPIO_PIN_5);
    
        //
        // The GPIO port and pins have been set up for CAN.  The CAN peripheral
        // must be enabled.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_CAN0);
    
        //
        // Initialize the CAN controller
        //
        CANInit(CAN0_BASE);
    
        //
        // Set up the bit rate for the CAN bus.  This function sets up the CAN
        // bus timing for a nominal configuration.  You can achieve more control
        // over the CAN bus timing by using the function CANBitTimingSet() instead
        // of this one, if needed.
        // In this example, the CAN bus is set to 500 kHz.  In the function below,
        // the call to SysCtlClockGet() or ui32SysClock is used to determine the 
    	// clock rate that is used for clocking the CAN peripheral.  This can be 
    	// replaced with a  fixed value if you know the value of the system clock, 
    	// saving the extra function call.  For some parts, the CAN peripheral is 
    	// clocked by a fixed 8 MHz regardless of the system clock in which case 
    	// the call to SysCtlClockGet() or ui32SysClock should be replaced with 
    	// 8000000.  Consult the data sheet for more information about CAN 
    	// peripheral clocking.
        //
    #if defined(TARGET_IS_TM4C129_RA0) ||                                         \
    	defined(TARGET_IS_TM4C129_RA1) ||                                         \
        defined(TARGET_IS_TM4C129_RA2)
        CANBitRateSet(CAN0_BASE, ui32SysClock, 500000);
    #else
        CANBitRateSet(CAN0_BASE, SysCtlClockGet(), 500000);
    #endif
    
        //
        // Enable interrupts on the CAN peripheral.  This example uses static
        // allocation of interrupt handlers which means the name of the handler
        // is in the vector table of startup code.  If you want to use dynamic
        // allocation of the vector table, then you must also call CANIntRegister()
        // here.
        //
        // CANIntRegister(CAN0_BASE, CANIntHandler); // if using dynamic vectors
        //
        CANIntEnable(CAN0_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS);
    
        //
        // Enable the CAN interrupt on the processor (NVIC).
        //
        IntEnable(INT_CAN0);
    
        //
        // Enable the CAN for operation.
        //
        CANEnable(CAN0_BASE);
    
        //
        // Initialize the message object that will be used for sending CAN
        // messages.  The message will be 4 bytes that will contain an incrementing
        // value.  Initially it will be set to 0.
        //
    
        //
        // Initialize message object 1 to be able to send CAN message 1.  This
        // message object is not shared so it only needs to be initialized one
        // time, and can be used for repeatedly sending the same message ID.
        //
        g_sCANMsgObject1.ui32MsgID = 0x1001;
        g_sCANMsgObject1.ui32MsgIDMask = 0;
        g_sCANMsgObject1.ui32Flags = MSG_OBJ_TX_INT_ENABLE;
        g_sCANMsgObject1.ui32MsgLen = sizeof(g_pui8Msg1);
        g_sCANMsgObject1.pui8MsgData = g_pui8Msg1;
    
        //
        // Initialize message object 2 to be able to send CAN message 2.  This
        // message object is not shared so it only needs to be initialized one
        // time, and can be used for repeatedly sending the same message ID.
        //
        g_sCANMsgObject2.ui32MsgID = 0x2001;
        g_sCANMsgObject2.ui32MsgIDMask = 0;
        g_sCANMsgObject2.ui32Flags = MSG_OBJ_TX_INT_ENABLE;
        g_sCANMsgObject2.ui32MsgLen = sizeof(g_pui8Msg2);
        g_sCANMsgObject2.pui8MsgData = g_pui8Msg2;
    
        //
        // Enter loop to send messages.  Four messages will be sent once per
        // second.  The contents of each message will be changed each time.
        //
        for(;;)
        {
            //
            // Send message 1 using CAN controller message object 1.  This is
            // the only message sent using this message object.  The
            // CANMessageSet() function will cause the message to be sent right
            // away.
            //
            PrintCANMessageInfo(&g_sCANMsgObject1, 1);
            CANMessageSet(CAN0_BASE, 1, &g_sCANMsgObject1, MSG_OBJ_TYPE_TX);
    
            //
            // Send message 2 using CAN controller message object 2.  This is
            // the only message sent using this message object.  The
            // CANMessageSet() function will cause the message to be sent right
            // away.
            //
            PrintCANMessageInfo(&g_sCANMsgObject2, 2);
            CANMessageSet(CAN0_BASE, 2, &g_sCANMsgObject2, MSG_OBJ_TYPE_TX);
    
            //
            // Load message object 3 with message 3.  This is needs to be done each
            // time because message object 3 is being shared for two different
            // messages.
            //
            g_sCANMsgObject3.ui32MsgID = 0x3001;
            g_sCANMsgObject3.ui32MsgIDMask = 0;
            g_sCANMsgObject3.ui32Flags = MSG_OBJ_TX_INT_ENABLE;
            g_sCANMsgObject3.ui32MsgLen = sizeof(g_pui8Msg3);
            g_sCANMsgObject3.pui8MsgData = g_pui8Msg3;
    
            //
            // Clear the flag that indicates that message 3 has been sent.  This
            // flag will be set in the interrupt handler when a message has been
            // sent using message object 3.
            //
            g_bMsgObj3Sent = 0;
    
            //
            // Now send message 3 using CAN controller message object 3.  This is
            // the first message sent using this message object.  The
            // CANMessageSet() function will cause the message to be sent right
            // away.
            //
            PrintCANMessageInfo(&g_sCANMsgObject3, 3);
            CANMessageSet(CAN0_BASE, 3, &g_sCANMsgObject3, MSG_OBJ_TYPE_TX);
    
            //
            // Wait for the indication from the interrupt handler that message
            // object 3 is done, because we are re-using it for another message.
            //
            while(!g_bMsgObj3Sent)
            {
            }
    
            //
            // Load message object 3 with message 4.  This is needed because
            // message object 3 is being shared for two different messages.
            //
            g_sCANMsgObject3.ui32MsgID = 0x3002;
            g_sCANMsgObject3.ui32MsgIDMask = 0;
            g_sCANMsgObject3.ui32Flags = MSG_OBJ_TX_INT_ENABLE;
            g_sCANMsgObject3.ui32MsgLen = sizeof(g_pui8Msg4);
            g_sCANMsgObject3.pui8MsgData = g_pui8Msg4;
    
            //
            // Now send message 4 using CAN controller message object 3.  This is
            // the second message sent using this message object.  The
            // CANMessageSet() function will cause the message to be sent right
            // away.
            //
            PrintCANMessageInfo(&g_sCANMsgObject3, 3);
            CANMessageSet(CAN0_BASE, 3, &g_sCANMsgObject3, MSG_OBJ_TYPE_TX);
    
            //
            // Wait 1 second before continuing
            //
            SimpleDelay();
    
            //
            // Check the error flag to see if errors occurred
            //
            if(g_bErrFlag)
            {
                UARTprintf(" error - cable connected?\n");
            }
            else
            {
                //
                // If no errors then print the count of message sent
                //
                UARTprintf(" total count = %u\n",
                           g_ui32Msg1Count + g_ui32Msg2Count + g_ui32Msg3Count);
            }
    
            //
            // Change the value in the message data for each of the messages.
            //
            (*(uint32_t *)g_pui8Msg1)++;
            (*(uint32_t *)g_pui8Msg2)++;
            (*(uint32_t *)g_pui8Msg3)++;
            (*(uint32_t *)&g_pui8Msg4[0])++;
            (*(uint32_t *)&g_pui8Msg4[4])--;
        }
    
        //
        // Return no errors
        //
        return(0);
    }
    
    hello amit,

    I have attached the code . sorry for the delay. I am actually using the micro controller for reception and SAINT 2 BOX for transmission. The problem is the msg ID on the transmission side is different and the receiver code it is different , and yet the message is received. how is it happening ?

    Regards,

    Monica

  • Hello Monica,

    I am not sure what is the Msg ID on the TX side and RX side being received (no indication of that in the post) nor who is the TX and who is the RX. Please clarify,

    Regards
    Amit
  • hello amit,

    I am using a code where once a message is received it has to identify the service ID from the message( i have initialized the ID as 11) and if the ID corresponds to the requirement it has to go into the loop and it has to send the required DTC(diagnostic trouble codes). So in the same program i have created a function . If the ID is same then go into the loop where i have initialized another message object for transmission of DTC.The ID gets printed after that it does not go into the loop for transmission. It says the message object is declared but not referenced. I have attached the code.

    Thanking you.

    Monica G V

    //*****************************************************************************
    //
    // multi_rx.c - Peripheral example demonstrating multiple CAN message
    //              reception.
    //
    // Copyright (c) 2010-2015 Texas Instruments Incorporated.  All rights reserved.
    // Software License Agreement
    // 
    //   Redistribution and use in source and binary forms, with or without
    //   modification, are permitted provided that the following conditions
    //   are met:
    // 
    //   Redistributions of source code must retain the above copyright
    //   notice, this list of conditions and the following disclaimer.
    // 
    //   Redistributions in binary form must reproduce the above copyright
    //   notice, this list of conditions and the following disclaimer in the
    //   documentation and/or other materials provided with the  
    //   distribution.
    // 
    //   Neither the name of Texas Instruments Incorporated nor the names of
    //   its contributors may be used to endorse or promote products derived
    //   from this software without specific prior written permission.
    // 
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // 
    // This is part of revision 2.1.1.71 of the Tiva Firmware Development Package.
    //
    //*****************************************************************************
    
    #include <stdbool.h>
    #include <stdint.h>
    #include "inc/hw_can.h"
    #include "inc/hw_memmap.h"
    #include "inc/hw_ints.h"
    #include "driverlib/can.h"
    #include "driverlib/gpio.h"
    #include "driverlib/interrupt.h"
    #include "driverlib/pin_map.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/uart.h"
    #include "utils/uartstdio.h"
    
    //*****************************************************************************
    //
    //! \addtogroup can_examples_list
    //! <h1>Multiple CAN RX (multi_rx)</h1>
    //!
    //! This example shows how to set up the CAN to receive multiple CAN messages
    //! using separate message objects for different messages, and using CAN ID
    //! filtering to control which messages are received.  Three message objects
    //! are set up to receive 3 of the 4 CAN message IDs that are used by the
    //! multi_tx example.  Filtering is used to demonstrate how to receive only
    //! specific messages, and therefore not receiving all 4 messages from the
    //! multi_tx example.  As messages are received the content of each are printed
    //! to the serial console.
    //!
    //! This example uses the following peripherals and I/O signals.  You must
    //! review these and change as needed for your own board:
    //! - CAN0 peripheral
    //! - GPIO port B peripheral (for CAN0 pins)
    //! - CAN0RX - PB4
    //! - CAN0TX - PB5
    //!
    //! The following UART signals are configured only for displaying console
    //! messages for this example.  These are not required for operation of CAN.
    //! - GPIO port A peripheral (for UART0 pins)
    //! - UART0RX - PA0
    //! - UART0TX - PA1
    //!
    //! This example uses the following interrupt handlers.  To use this example
    //! in your own application you must add these interrupt handlers to your
    //! vector table.
    //! - INT_CAN0 - CANIntHandler
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // A counter that keeps track of the number of times the RX interrupt has
    // occurred, which should match the number of messages that were received.
    //
    //*****************************************************************************
    volatile uint32_t g_ui32MsgCount = 0;
     unsigned int X[30];
     unsigned int uIdx;
     /*extern void gettingmsg(tCANMsgObject *psCANMsg, uint32_t ui32MsgObj);*/
    //*****************************************************************************
    //
    // A flag for the interrupt handler to indicate that a message was received.
    //
    //*****************************************************************************
    volatile bool g_bRXFlag1 = 0;
    
    //*****************************************************************************
    //
    // A flag to indicate that some reception error occurred.
    //
    //*****************************************************************************
    volatile bool g_bErrFlag = 0;
    
    
    //*****************************************************************************
    //
    // This function sets up UART0 to be used for a console to display information
    // as the example is running.
    
    tCANMsgObject g_SCANMsgObject2;
    
    uint8_t g_pui8Msg[8]={ 03,51, 01, 00, 00, 00, 00, 00};
    
    //
    //*****************************************************************************
    void
    InitConsole(void)
    {
        //
        // Enable GPIO port A which is used for UART0 pins.
        // TODO: change this to whichever GPIO port you are using.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
    
        //
        // Configure the pin muxing for UART0 functions on port A0 and A1.
        // This step is not necessary if your part does not support pin muxing.
        // TODO: change this to select the port/pin you are using.
        //
        GPIOPinConfigure(GPIO_PA0_U0RX);
        GPIOPinConfigure(GPIO_PA1_U0TX);
    
        //
        // Enable UART0 so that we can configure the clock.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
    
        //
        // Use the internal 16MHz oscillator as the UART clock source.
        //
        UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
    
        //
        // Select the alternate (UART) function for these pins.
        // TODO: change this to select the port/pin you are using.
        //
        GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
    
        //
        // Initialize the UART for console I/O.
        //
        UARTStdioConfig(0, 115200, 16000000);
    }
    
    
    
    
    
    
    
    
    
    
    
    //*****************************************************************************
    //
    // This function prints some information about the CAN message to the
    // serial port for information purposes only.
    //
    //*****************************************************************************
    void
    PrintCANMessageInfo(tCANMsgObject *psCANMsg, uint32_t ui32MsgObj)
    {
    
    
        //
        // Check to see if there is an indication that some messages were
        // lost.
        //
        if(psCANMsg->ui32Flags & MSG_OBJ_DATA_LOST)
        {
            UARTprintf("CAN message loss detected on message object %d\n",
                       ui32MsgObj);
        }
    
        //
        // Print out the contents of the message that was received.
        //
        UARTprintf("Msg Obj=%u ID=0x%05X len=%u data=0x", ui32MsgObj,
                   psCANMsg->ui32MsgID, psCANMsg->ui32MsgLen);
        for(uIdx = 0; uIdx < psCANMsg->ui32MsgLen; uIdx++)
        {
            UARTprintf("%02X ", psCANMsg->pui8MsgData[uIdx]);
    
        }
    
        UARTprintf("\n");
    
    
    }
    
    void
    PrintCANMessageInfo1(tCANMsgObject *psCANMsg, uint32_t ui32MsgObj)
    {
    
        UARTprintf("sending msg: Obj=%d ID=0x%05X data=0x", ui32MsgObj,
                   psCANMsg->ui32MsgID);
        for(uIdx = 0; uIdx < psCANMsg->ui32MsgLen; uIdx++)
        {
            UARTprintf("%02X ", psCANMsg->pui8MsgData[uIdx]);
    
        }
        UARTprintf("\n");
    }
    
    void gettingmsg(tCANMsgObject *psCANMsg, uint32_t ui32MsgObj)
             {
             	for(uIdx =0; uIdx < psCANMsg->ui32MsgLen; uIdx++)
             	       {
             	    	X[uIdx]=psCANMsg->pui8MsgData[uIdx];
             	       if(X[uIdx]==11)
             	                 {
    
    
             	    	 // initializing msg object 2 for transmission//
    
    
    
             	    	 // data to be transmitted //
    
    
             	    	            g_SCANMsgObject2.ui32MsgID = 0x2001;
             	    	             g_SCANMsgObject2.ui32MsgIDMask =0xff;
             	    	             g_SCANMsgObject2.ui32Flags = MSG_OBJ_TX_INT_ENABLE;
             	    	             g_SCANMsgObject2.ui32MsgLen = sizeof(g_pui8Msg);
             	    	             g_SCANMsgObject2.pui8MsgData = g_pui8Msg;
    
             	    	             CANMessageSet(CAN0_BASE, 2, &g_SCANMsgObject2, MSG_OBJ_TYPE_TX);
             	                     UARTprintf("%d",X[1]);
             	                     X[1]=0;
             	                     UARTprintf("\n");
    
    
    
    
    
             	                 }
             	       }
             }
    
    
    
    
    //*****************************************************************************
    //
    // This function is the interrupt handler for the CAN peripheral.  It checks
    // for the cause of the interrupt, and maintains a count of all messages that
    // have been received.
    //
    //*****************************************************************************
    ;
    CANIntHandler(void)
    {
        uint32_t ui32Status;
    
        //
        // Read the CAN interrupt status to find the cause of the interrupt
        //
        ui32Status = CANIntStatus(CAN0_BASE, CAN_INT_STS_CAUSE);
    
        //
        // If the cause is a controller status interrupt, then get the status
        //
        if(ui32Status == CAN_INT_INTID_STATUS)
        {
            //
            // Read the controller status.  This will return a field of status
            // error bits that can indicate various errors.  Error processing
            // is not done in this example for simplicity.  Refer to the
            // API documentation for details about the error status bits.
            // The act of reading this status will clear the interrupt.
            //
            ui32Status = CANStatusGet(CAN0_BASE, CAN_STS_CONTROL);
    
            //
            // Set a flag to indicate some errors may have occurred.
            //
            g_bErrFlag = 1;
        }
    
        //
        // Check if the cause is message object 1.
        //
        else if(ui32Status == 1)
        {
            //
            // Getting to this point means that the RX interrupt occurred on
            // message object 1, and the message reception is complete.  Clear the
            // message object interrupt.
            //
            CANIntClear(CAN0_BASE, 1);
    
            //
            // Increment a counter to keep track of how many messages have been
            // received.  In a real application this could be used to set flags to
            // indicate when a message is received.
            //
            g_ui32MsgCount++;
    
            //
            // Set flag to indicate received message is pending for this message
            // object.
            //
            g_bRXFlag1 = 1;
    
            //
            // Since a message was received, clear any error flags.
            //
            g_bErrFlag = 0;
        }
    
        //
        // Check if the cause is message object 2.
        //
    
        else
        {
            //
            // Spurious interrupt handling can go here.
            //
        }
    }
    
    //*****************************************************************************
    //
    // Configure the CAN and enter a loop to receive CAN messages.
    //
    //*****************************************************************************
    int
    main(void)
    {
    #if defined(TARGET_IS_TM4C129_RA0) ||                                         \
    	defined(TARGET_IS_TM4C129_RA1) ||                                         \
        defined(TARGET_IS_TM4C129_RA2)
    	uint32_t ui32SysClock;
    #endif
    
        tCANMsgObject sCANMessage;
        uint8_t pui8MsgData[8];
    
    
    
    
    
    
        //
        // Set the clocking to run directly from the external crystal/oscillator.
        // TODO: The SYSCTL_XTAL_ value must be changed to match the value of the
        // crystal used on your board.
        //
    #if defined(TARGET_IS_TM4C129_RA0) ||                                         \
    	defined(TARGET_IS_TM4C129_RA1) ||                                         \
        defined(TARGET_IS_TM4C129_RA2)
        ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
                                           SYSCTL_OSC_MAIN |
                                           SYSCTL_USE_OSC)
                                           25000000);
    #else
        SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
                       SYSCTL_XTAL_16MHZ);
    #endif
    
        //
        // Set up the serial console to use for displaying messages.  This is
        // just for this example program and is not needed for CAN operation.
        //
        InitConsole();
    
        //
        // For this example CAN0 is used with RX and TX pins on port B4 and B5.
        // The actual port and pins used may be different on your part, consult
        // the data sheet for more information.
        // GPIO port B needs to be enabled so these pins can be used.
        // TODO: change this to whichever GPIO port you are using
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
    
        //
        // Configure the GPIO pin muxing to select CAN0 functions for these pins.
        // This step selects which alternate function is available for these pins.
        // This is necessary if your part supports GPIO pin function muxing.
        // Consult the data sheet to see which functions are allocated per pin.
        // TODO: change this to select the port/pin you are using
        //
        GPIOPinConfigure(GPIO_PB4_CAN0RX);
        GPIOPinConfigure(GPIO_PB5_CAN0TX);
    
        //
        // Enable the alternate function on the GPIO pins.  The above step selects
        // which alternate function is available.  This step actually enables the
        // alternate function instead of GPIO for these pins.
        // TODO: change this to match the port/pin you are using
        //
        GPIOPinTypeCAN(GPIO_PORTB_BASE, GPIO_PIN_4 | GPIO_PIN_5);
    
        //
        // The GPIO port and pins have been set up for CAN.  The CAN peripheral
        // must be enabled.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_CAN0);
    
        //
        // Initialize the CAN controller
        //
        CANInit(CAN0_BASE);
    
        //
        // Set up the bit rate for the CAN bus.  This function sets up the CAN
        // bus timing for a nominal configuration.  You can achieve more control
        // over the CAN bus timing by using the function CANBitTimingSet() instead
        // of this one, if needed.
        // In this example, the CAN bus is set to 500 kHz.  In the function below,
        // the call to SysCtlClockGet() or ui32SysClock is used to determine the 
    	// clock rate that is used for clocking the CAN peripheral.  This can be 
    	// replaced with a  fixed value if you know the value of the system clock, 
    	// saving the extra function call.  For some parts, the CAN peripheral is 
    	// clocked by a fixed 8 MHz regardless of the system clock in which case 
    	// the call to SysCtlClockGet() or ui32SysClock should be replaced with 
    	// 8000000.  Consult the data sheet for more information about CAN 
    	// peripheral clocking.
        //
    #if defined(TARGET_IS_TM4C129_RA0) ||                                         \
    	defined(TARGET_IS_TM4C129_RA1) ||                                         \
        defined(TARGET_IS_TM4C129_RA2)
        CANBitRateSet(CAN0_BASE, ui32SysClock, 500000);
    #else
        CANBitRateSet(CAN0_BASE, SysCtlClockGet(), 500000);
    #endif
    
        //
        // Enable interrupts on the CAN peripheral.  This example uses static
        // allocation of interrupt handlers which means the name of the handler
        // is in the vector table of startup code.  If you want to use dynamic
        // allocation of the vector table, then you must also call CANIntRegister()
        // here.
        //
        // CANIntRegister(CAN0_BASE, CANIntHandler); // if using dynamic vectors
        //
        CANIntEnable(CAN0_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS);
    
        //
        // Enable the CAN interrupt on the processor (NVIC).
        //
        IntEnable(INT_CAN0);
    
        //
        // Enable the CAN for operation.
        //
        CANEnable(CAN0_BASE);
    
        //
        // Initialize a message object to receive CAN messages with ID 0x1001.
        // The expected ID must be set along with the mask to indicate that all
        // bits in the ID must match.
        //
        sCANMessage.ui32MsgID = 0x1001;
        sCANMessage.ui32MsgIDMask = 10;
        sCANMessage.ui32Flags = (MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER |
                                 MSG_OBJ_EXTENDED_ID);
        sCANMessage.ui32MsgLen = 8;
    
        //
        // Now load the message object into the CAN peripheral message object 1.
        // Once loaded the CAN will receive any messages with this CAN ID into
        // this message object, and an interrupt will occur.
        //
        CANMessageSet(CAN0_BASE, 1, &sCANMessage, MSG_OBJ_TYPE_RX);
    
        //
        // Change the ID to 0x2001, and load into message object 2 which will be
        // used for receiving any CAN messages with this ID.  Since only the CAN
        // ID field changes, we don't need to reload all the other fields.
        //
    
    
    
        for(;;)
        {
            //
            // If the flag for message object 1 is set, that means that the RX
            // interrupt occurred and there is a message ready to be read from
            // this CAN message object.
            //
            if(g_bRXFlag1)
            {
                //
                // Reuse the same message object that was used earlier to configure
                // the CAN for receiving messages.  A buffer for storing the
                // received data must also be provided, so set the buffer pointer
                // within the message object.  This same buffer is used for all
                // messages in this example, but your application could set a
                // different buffer each time a message is read in order to store
                // different messages in different buffers.
                //
                sCANMessage.pui8MsgData = pui8MsgData;
    
                //
                // Read the message from the CAN.  Message object number 1 is used
                // (which is not the same thing as CAN ID).  The interrupt clearing
                // flag is not set because this interrupt was already cleared in
                // the interrupt handler.
                //
                CANMessageGet(CAN0_BASE, 1, &sCANMessage, 0);
    
                //
                // Clear the pending message flag so that the interrupt handler can
                // set it again when the next message arrives.
                //
                g_bRXFlag1 = 0;
    
                //
                // Print information about the message just received.
                //
                PrintCANMessageInfo(&sCANMessage, 1);
                gettingmsg(&sCANMessage, 1);
    
    	      //  PrintCANMessageInfo1(&g_SCANMsgObject2, 2);
    
    
    
            }
            }
    
    
    
            //
            // Check for message received on message object 2.  If so then
            // read message and print information.
            //
    
        }
    
    

  • hello amit,
    Also i have set message object with objID 1 to receive. Using CANmessageGet function the message is read.So now in the same program can i again initialize it to transmit the data?
  • Hello Monica

    You can use the Object ID with a Transmit object but note that the RX path shall receive the same as the RX object has the same message ID filter.

    Regards
    Amit
  • Hello amit
    Regarding the code what was the problem .where have I gone wrong .
    Thanking you
    Monica
  • Hello Monica

    Where is the Interrupt Handler which is handling the TX messages in the code? Also are you able to see the message on the bus?

    Regards
    Amit
  • //*****************************************************************************
    //
    // multi_rx.c - Peripheral example demonstrating multiple CAN message
    //              reception.
    //
    // Copyright (c) 2010-2015 Texas Instruments Incorporated.  All rights reserved.
    // Software License Agreement
    // 
    //   Redistribution and use in source and binary forms, with or without
    //   modification, are permitted provided that the following conditions
    //   are met:
    // 
    //   Redistributions of source code must retain the above copyright
    //   notice, this list of conditions and the following disclaimer.
    // 
    //   Redistributions in binary form must reproduce the above copyright
    //   notice, this list of conditions and the following disclaimer in the
    //   documentation and/or other materials provided with the  
    //   distribution.
    // 
    //   Neither the name of Texas Instruments Incorporated nor the names of
    //   its contributors may be used to endorse or promote products derived
    //   from this software without specific prior written permission.
    // 
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // 
    // This is part of revision 2.1.1.71 of the Tiva Firmware Development Package.
    //
    //*****************************************************************************
    
    #include <stdbool.h>
    #include <stdint.h>
    #include "inc/hw_can.h"
    #include "inc/hw_memmap.h"
    #include "inc/hw_ints.h"
    #include "driverlib/can.h"
    #include "driverlib/gpio.h"
    #include "driverlib/interrupt.h"
    #include "driverlib/pin_map.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/uart.h"
    #include "utils/uartstdio.h"
    
    //*****************************************************************************
    //
    //! \addtogroup can_examples_list
    //! <h1>Multiple CAN RX (multi_rx)</h1>
    //!
    //! This example shows how to set up the CAN to receive multiple CAN messages
    //! using separate message objects for different messages, and using CAN ID
    //! filtering to control which messages are received.  Three message objects
    //! are set up to receive 3 of the 4 CAN message IDs that are used by the
    //! multi_tx example.  Filtering is used to demonstrate how to receive only
    //! specific messages, and therefore not receiving all 4 messages from the
    //! multi_tx example.  As messages are received the content of each are printed
    //! to the serial console.
    //!
    //! This example uses the following peripherals and I/O signals.  You must
    //! review these and change as needed for your own board:
    //! - CAN0 peripheral
    //! - GPIO port B peripheral (for CAN0 pins)
    //! - CAN0RX - PB4
    //! - CAN0TX - PB5
    //!
    //! The following UART signals are configured only for displaying console
    //! messages for this example.  These are not required for operation of CAN.
    //! - GPIO port A peripheral (for UART0 pins)
    //! - UART0RX - PA0
    //! - UART0TX - PA1
    //!
    //! This example uses the following interrupt handlers.  To use this example
    //! in your own application you must add these interrupt handlers to your
    //! vector table.
    //! - INT_CAN0 - CANIntHandler
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // A counter that keeps track of the number of times the RX interrupt has
    // occurred, which should match the number of messages that were received.
    //
    //*****************************************************************************
    volatile uint32_t g_ui32MsgCount = 0;
     unsigned int X[30];
     unsigned int uIdx;
     /*extern void gettingmsg(tCANMsgObject *psCANMsg, uint32_t ui32MsgObj);*/
    //*****************************************************************************
    //
    // A flag for the interrupt handler to indicate that a message was received.
    //
    //*****************************************************************************
    volatile bool g_bRXFlag1 = 0;
    
    //*****************************************************************************
    //
    // A flag to indicate that some reception error occurred.
    //
    //*****************************************************************************
    volatile bool g_bErrFlag = 0;
    
    
    //*****************************************************************************
    //
    // This function sets up UART0 to be used for a console to display information
    // as the example is running.
    
    tCANMsgObject g_SCANMsgObject2;
    
    uint8_t g_pui8Msg[8]={ 03,51, 01, 00, 00, 00, 00, 00};
    
    //
    //*****************************************************************************
    void
    InitConsole(void)
    {
        //
        // Enable GPIO port A which is used for UART0 pins.
        // TODO: change this to whichever GPIO port you are using.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
    
        //
        // Configure the pin muxing for UART0 functions on port A0 and A1.
        // This step is not necessary if your part does not support pin muxing.
        // TODO: change this to select the port/pin you are using.
        //
        GPIOPinConfigure(GPIO_PA0_U0RX);
        GPIOPinConfigure(GPIO_PA1_U0TX);
    
        //
        // Enable UART0 so that we can configure the clock.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
    
        //
        // Use the internal 16MHz oscillator as the UART clock source.
        //
        UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
    
        //
        // Select the alternate (UART) function for these pins.
        // TODO: change this to select the port/pin you are using.
        //
        GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
    
        //
        // Initialize the UART for console I/O.
        //
        UARTStdioConfig(0, 115200, 16000000);
    }
    
    
    
    
    
    
    
    
    
    
    
    //*****************************************************************************
    //
    // This function prints some information about the CAN message to the
    // serial port for information purposes only.
    //
    //*****************************************************************************
    void
    PrintCANMessageInfo(tCANMsgObject *psCANMsg, uint32_t ui32MsgObj)
    {
    
    
        //
        // Check to see if there is an indication that some messages were
        // lost.
        //
        if(psCANMsg->ui32Flags & MSG_OBJ_DATA_LOST)
        {
            UARTprintf("CAN message loss detected on message object %d\n",
                       ui32MsgObj);
        }
    
        //
        // Print out the contents of the message that was received.
        //
        UARTprintf("Msg Obj=%u ID=0x%05X len=%u data=0x", ui32MsgObj,
                   psCANMsg->ui32MsgID, psCANMsg->ui32MsgLen);
        for(uIdx = 0; uIdx < psCANMsg->ui32MsgLen; uIdx++)
        {
            UARTprintf("%02X ", psCANMsg->pui8MsgData[uIdx]);
    
        }
    
        UARTprintf("\n");
    
    
    }
    
    void
    PrintCANMessageInfo1(tCANMsgObject *psCANMsg, uint32_t ui32MsgObj)
    {
    
        UARTprintf("sending msg: Obj=%d ID=0x%05X data=0x", ui32MsgObj,
                   psCANMsg->ui32MsgID);
        for(uIdx = 0; uIdx < psCANMsg->ui32MsgLen; uIdx++)
        {
            UARTprintf("%02X ", psCANMsg->pui8MsgData[uIdx]);
    
        }
        UARTprintf("\n");
    }
    
    void gettingmsg(tCANMsgObject *psCANMsg, uint32_t ui32MsgObj)
             {
             	for(uIdx =0; uIdx < psCANMsg->ui32MsgLen; uIdx++)
             	       {
             	    	X[uIdx]=psCANMsg->pui8MsgData[uIdx];
             	       if(X[uIdx]==11)
             	                 {
    
    
             	    	 // initializing msg object 2 for transmission//
    
    
    
             	    	 // data to be transmitted //
    
    
             	    	            g_SCANMsgObject2.ui32MsgID = 0x2001;
             	    	             g_SCANMsgObject2.ui32MsgIDMask =0xff;
             	    	             g_SCANMsgObject2.ui32Flags = MSG_OBJ_TX_INT_ENABLE;
             	    	             g_SCANMsgObject2.ui32MsgLen = sizeof(g_pui8Msg);
             	    	             g_SCANMsgObject2.pui8MsgData = g_pui8Msg;
    
             	    	             CANMessageSet(CAN0_BASE, 2, &g_SCANMsgObject2, MSG_OBJ_TYPE_TX);
             	                     UARTprintf("%d",X[1]);
             	                     X[1]=0;
             	                     UARTprintf("\n");
    
    
    
    
    
             	                 }
             	       }
             }
    
    
    
    
    //*****************************************************************************
    //
    // This function is the interrupt handler for the CAN peripheral.  It checks
    // for the cause of the interrupt, and maintains a count of all messages that
    // have been received.
    //
    //*****************************************************************************
    ;
    CANIntHandler(void)
    {
        uint32_t ui32Status;
    
        //
        // Read the CAN interrupt status to find the cause of the interrupt
        //
        ui32Status = CANIntStatus(CAN0_BASE, CAN_INT_STS_CAUSE);
    
        //
        // If the cause is a controller status interrupt, then get the status
        //
        if(ui32Status == CAN_INT_INTID_STATUS)
        {
            //
            // Read the controller status.  This will return a field of status
            // error bits that can indicate various errors.  Error processing
            // is not done in this example for simplicity.  Refer to the
            // API documentation for details about the error status bits.
            // The act of reading this status will clear the interrupt.
            //
            ui32Status = CANStatusGet(CAN0_BASE, CAN_STS_CONTROL);
    
            //
            // Set a flag to indicate some errors may have occurred.
            //
            g_bErrFlag = 1;
        }
    
        //
        // Check if the cause is message object 1.
        //
        else if(ui32Status == 1)
        {
            //
            // Getting to this point means that the RX interrupt occurred on
            // message object 1, and the message reception is complete.  Clear the
            // message object interrupt.
            //
            CANIntClear(CAN0_BASE, 1);
    
            //
            // Increment a counter to keep track of how many messages have been
            // received.  In a real application this could be used to set flags to
            // indicate when a message is received.
            //
            g_ui32MsgCount++;
    
            //
            // Set flag to indicate received message is pending for this message
            // object.
            //
            g_bRXFlag1 = 1;
    
            //
            // Since a message was received, clear any error flags.
            //
            g_bErrFlag = 0;
        }
    
        //
        // Check if the cause is message object 2.
        //
    
        else
        {
            //
            // Spurious interrupt handling can go here.
            //
        }
    }
    
    //*****************************************************************************
    //
    // Configure the CAN and enter a loop to receive CAN messages.
    //
    //*****************************************************************************
    int
    main(void)
    {
    #if defined(TARGET_IS_TM4C129_RA0) ||                                         \
    	defined(TARGET_IS_TM4C129_RA1) ||                                         \
        defined(TARGET_IS_TM4C129_RA2)
    	uint32_t ui32SysClock;
    #endif
    
        tCANMsgObject sCANMessage;
        uint8_t pui8MsgData[8];
    
    
    
    
    
    
        //
        // Set the clocking to run directly from the external crystal/oscillator.
        // TODO: The SYSCTL_XTAL_ value must be changed to match the value of the
        // crystal used on your board.
        //
    #if defined(TARGET_IS_TM4C129_RA0) ||                                         \
    	defined(TARGET_IS_TM4C129_RA1) ||                                         \
        defined(TARGET_IS_TM4C129_RA2)
        ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
                                           SYSCTL_OSC_MAIN |
                                           SYSCTL_USE_OSC)
                                           25000000);
    #else
        SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
                       SYSCTL_XTAL_16MHZ);
    #endif
    
        //
        // Set up the serial console to use for displaying messages.  This is
        // just for this example program and is not needed for CAN operation.
        //
        InitConsole();
    
        //
        // For this example CAN0 is used with RX and TX pins on port B4 and B5.
        // The actual port and pins used may be different on your part, consult
        // the data sheet for more information.
        // GPIO port B needs to be enabled so these pins can be used.
        // TODO: change this to whichever GPIO port you are using
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
    
        //
        // Configure the GPIO pin muxing to select CAN0 functions for these pins.
        // This step selects which alternate function is available for these pins.
        // This is necessary if your part supports GPIO pin function muxing.
        // Consult the data sheet to see which functions are allocated per pin.
        // TODO: change this to select the port/pin you are using
        //
        GPIOPinConfigure(GPIO_PB4_CAN0RX);
        GPIOPinConfigure(GPIO_PB5_CAN0TX);
    
        //
        // Enable the alternate function on the GPIO pins.  The above step selects
        // which alternate function is available.  This step actually enables the
        // alternate function instead of GPIO for these pins.
        // TODO: change this to match the port/pin you are using
        //
        GPIOPinTypeCAN(GPIO_PORTB_BASE, GPIO_PIN_4 | GPIO_PIN_5);
    
        //
        // The GPIO port and pins have been set up for CAN.  The CAN peripheral
        // must be enabled.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_CAN0);
    
        //
        // Initialize the CAN controller
        //
        CANInit(CAN0_BASE);
    
        //
        // Set up the bit rate for the CAN bus.  This function sets up the CAN
        // bus timing for a nominal configuration.  You can achieve more control
        // over the CAN bus timing by using the function CANBitTimingSet() instead
        // of this one, if needed.
        // In this example, the CAN bus is set to 500 kHz.  In the function below,
        // the call to SysCtlClockGet() or ui32SysClock is used to determine the 
    	// clock rate that is used for clocking the CAN peripheral.  This can be 
    	// replaced with a  fixed value if you know the value of the system clock, 
    	// saving the extra function call.  For some parts, the CAN peripheral is 
    	// clocked by a fixed 8 MHz regardless of the system clock in which case 
    	// the call to SysCtlClockGet() or ui32SysClock should be replaced with 
    	// 8000000.  Consult the data sheet for more information about CAN 
    	// peripheral clocking.
        //
    #if defined(TARGET_IS_TM4C129_RA0) ||                                         \
    	defined(TARGET_IS_TM4C129_RA1) ||                                         \
        defined(TARGET_IS_TM4C129_RA2)
        CANBitRateSet(CAN0_BASE, ui32SysClock, 500000);
    #else
        CANBitRateSet(CAN0_BASE, SysCtlClockGet(), 500000);
    #endif
    
        //
        // Enable interrupts on the CAN peripheral.  This example uses static
        // allocation of interrupt handlers which means the name of the handler
        // is in the vector table of startup code.  If you want to use dynamic
        // allocation of the vector table, then you must also call CANIntRegister()
        // here.
        //
        // CANIntRegister(CAN0_BASE, CANIntHandler); // if using dynamic vectors
        //
        CANIntEnable(CAN0_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS);
    
        //
        // Enable the CAN interrupt on the processor (NVIC).
        //
        IntEnable(INT_CAN0);
    
        //
        // Enable the CAN for operation.
        //
        CANEnable(CAN0_BASE);
    
        //
        // Initialize a message object to receive CAN messages with ID 0x1001.
        // The expected ID must be set along with the mask to indicate that all
        // bits in the ID must match.
        //
        sCANMessage.ui32MsgID = 0x1001;
        sCANMessage.ui32MsgIDMask = 10;
        sCANMessage.ui32Flags = (MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER |
                                 MSG_OBJ_EXTENDED_ID);
        sCANMessage.ui32MsgLen = 8;
    
        //
        // Now load the message object into the CAN peripheral message object 1.
        // Once loaded the CAN will receive any messages with this CAN ID into
        // this message object, and an interrupt will occur.
        //
        CANMessageSet(CAN0_BASE, 1, &sCANMessage, MSG_OBJ_TYPE_RX);
    
        //
        // Change the ID to 0x2001, and load into message object 2 which will be
        // used for receiving any CAN messages with this ID.  Since only the CAN
        // ID field changes, we don't need to reload all the other fields.
        //
    
    
    
        for(;;)
        {
            //
            // If the flag for message object 1 is set, that means that the RX
            // interrupt occurred and there is a message ready to be read from
            // this CAN message object.
            //
            if(g_bRXFlag1)
            {
                //
                // Reuse the same message object that was used earlier to configure
                // the CAN for receiving messages.  A buffer for storing the
                // received data must also be provided, so set the buffer pointer
                // within the message object.  This same buffer is used for all
                // messages in this example, but your application could set a
                // different buffer each time a message is read in order to store
                // different messages in different buffers.
                //
                sCANMessage.pui8MsgData = pui8MsgData;
    
                //
                // Read the message from the CAN.  Message object number 1 is used
                // (which is not the same thing as CAN ID).  The interrupt clearing
                // flag is not set because this interrupt was already cleared in
                // the interrupt handler.
                //
                CANMessageGet(CAN0_BASE, 1, &sCANMessage, 0);
    
                //
                // Clear the pending message flag so that the interrupt handler can
                // set it again when the next message arrives.
                //
                g_bRXFlag1 = 0;
    
                //
                // Print information about the message just received.
                //
                PrintCANMessageInfo(&sCANMessage, 1);
                gettingmsg(&sCANMessage, 1);
    
    	      //  PrintCANMessageInfo1(&g_SCANMsgObject2, 2);
    
    
    
            }
            }
    
    
    
            //
            // Check for message received on message object 2.  If so then
            // read message and print information.
            //
    
        }
    
    
    hello amit,

    I am using a code where once a message is received it has to identify the service ID from the message( i have initialized the ID as 11) and if the ID corresponds to the requirement it has to go into the loop and it has to send the required DTC(diagnostic trouble codes). So in the same program i have created a function . If the ID is same then go into the loop where i have initialized another message object for transmission of DTC.The ID gets printed after that it does not go into the loop for transmission. It says the message object is declared but not referenced. I have attached the code.

    Thanking you.

    Monica G V

  • yeah i tried doing that also. I did include an interrupt handler for transmission. I used saint box to monitor the message but i cant see any message on the bus.
  • Hello Monica,

    In the code file you sent I see the following

    ;
    CANIntHandler(void)

    which must be
    void
    CANIntHandler(void)

    Secondly, after making the change I compiled the code and it does not give any warning during compilation or link in my CCSv6.1 ARM Compiler v5.2.6.

    Regards
    Amit
  • Hello amit,
    I tried making the following changes , there were no warnings. Is it actually possible to configure another message object and transmit the data within the same receiver code? . If the code and initialization of another message object is correct why is the data not being transmitted. After reception when gettingmsg function is being called it should go into the loop . The uIdx[1]=11 it prints the data ,but that initialization of message object is not referenced.


    void gettingmsg(tCANMsgObject *psCANMsg, uint32_t ui32MsgObj)
    {
    for(uIdx =0; uIdx < psCANMsg->ui32MsgLen; uIdx++)
    {
    X[uIdx]=psCANMsg->pui8MsgData[uIdx];
    if(X[uIdx]==11)
    {
    // initializing message object 2 for transmission//
    // data to be transmitted //
    g_SCANMsgObject2.ui32MsgID = 0x2001;
    g_SCANMsgObject2.ui32MsgIDMask =0xff;
    g_SCANMsgObject2.ui32Flags = MSG_OBJ_TX_INT_ENABLE;
    g_SCANMsgObject2.ui32MsgLen = sizeof(g_pui8Msg);
    g_SCANMsgObject2.pui8MsgData = g_pui8Msg;

    CANMessageSet(CAN0_BASE, 2, &g_SCANMsgObject2, MSG_OBJ_TYPE_TX);
    UARTprintf("%d",X[1]);
    X[1]=0;
    UARTprintf("\n")
    }}}

    void
    PrintCANMessageInfo1(tCANMsgObject *psCANMsg, uint32_t ui32MsgObj)
    {

    UARTprintf("sending msg: Obj=%d ID=0x%05X data=0x", ui32MsgObj,
    psCANMsg->ui32MsgID);
    for(uIdx = 0; uIdx < psCANMsg->ui32MsgLen; uIdx++)
    {
    UARTprintf("%02X ", psCANMsg->pui8MsgData[uIdx]);

    }
    UARTprintf("\n");
    }



    Regards,
    Monica G V
  • Hello Monica,

    Can you please share the CCS project as I would need to run it on my setup to see what is happening?

    Regards,
    Amit
  • 6102.imp.zipHello amit,

    I have attached the ccs project.Sorry for the delay. Important.c is the receiver code and multi.tx is the transmission code. Its the receiver code that i am working with now. The initialization of second message object needs to be checked within the function void gettingmsg.

    Thanking you

    Monica

  • Hello amit,

    I have attached the .zip file after making few changes. How to do code partition?( That is after a particular message is being received we need to respond back .A transmission within a reception program). please help me through this. The interrupt handlers should be created again for the transmission ?? As i only initialized another message object inside a function and called it. Should we configure CAN and UART again?

    Thanking you4762.Current.zip

    Monica