Other Parts Discussed in Thread: EK-TM4C123GXL
I'm trying to power my Tiva C module using a 5V step down regulator which is connected to a 9V battery.
The Tiva C is connect to a BlueSMiRF to the following ports
UART1 Rx
UART1 Tx
3.3V output
And an Xbee series 1 to the following ports
UART5 Rx
UART5 Tx
3.3V output
The Xbee and the BlueSMiRF power up when I connect the 9V battery, but the LED flicker from the Tiva C doesn't turn on, nor does the code work.
I'm not sure if it's a current thing or grounding problem because when I connect the battery to the Tiva C and the Tiva C's USB port to the computer, everything works correctly (But both the battery and the serial USB connection have to be connected.