Other Parts Discussed in Thread: TM4C1294KCPDT
Hi,
I redesigned a touch screen device that was using Stellaris MCU to work with TIva MCU- TM4C1294KCPDT .
3.3 V (500mA) at the output of regulator and 3.3 V supply at all points near the Tiva is correct with out the Tiva on board. Once Tiva is soldered on to the board , and when the board is powered up ,the 3.3 V supply drops to 2.6 V at all points. Tiva gets really hot ,and I have not been able to program the board.
Ethernet ,SPI1,UART0, USB and Analog I/O are used. Port A pins used as UART /SPI and are not directly connected to ground. Port B is not used No connection. ( GPIO #9 issue mentioned in errata)
The datasheet recommends all unused pins to be grounded ,but all unused pins are NC
I have checked for shorts between pins, any chances for static discharge , changed the Tiva on board 3 times. What could be the reason for this heating and voltage drop issue ?
I was not sure if it is worth trying to program when the supply is less than 2.9 V ,still tried . The error obtained is
CORTEX_M3_0: GEL Output:
Memory Map Initialization Complete
CS_DAP_0: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 0.0.0.0)
Thanks,
Chandana