Other Parts Discussed in Thread: BOOSTXL-K350QVG-S1
I bought the Booster from Mouser Electronics with the following details: K350QVG-V2-F Lot: MAEBIT04 I am trying to interface to stellaris –launchpad EK-LM4F120XL with no success thus far. Driver that comes with the grlib demo program is Kentec320x240x16_ssd2119_8bit.c and the introduction suggests it is written for a parallel interface to SSD2119. PS3 = 0 PS2 = 0 PS1 = 1 PS2 = 1 //Kentec320x240x16_ssd2119_8bit.c - Display driver for the Kentec // K350QVG-V2-F TFT display with an SSD2119 // controller. This version assumes an // 8080-8bit interface between the micro // and display (PS3-0 = 0011b). The physical board has PS3- PS0 all connected to 3.3V (PS3-0 = 1111b) and that would suggest a 4-wire SPI interface What am I missing?