Hello,
we are using TMS470R1B1MPGEA controller for our application.
But we are not able to read/write the RAM/FLASH.
I have read the data from MSMPWL it shows data 0x00000000.
the MSMSCR register has the value 0x00000501;
My questions are as below,
1) The value of the MSMPWL is 0x00000000. by default the value has to be 0xffffffff. we have not changed the values?
2) How to make memory not secure?
3) Without MSM configuration can we access the RAM and Flash?
We are aware that TMS470R1B1MPGEA is not advisable to use, but we have custom board, need the help.
Thanks And Regards,
Vijay Hiremath