This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS31HDK GCC OperatingSystem : Setup



Hi,


I have TMS570LS31HDK board. Currently I am using CCS to connect, flash and debug on the board.

I have DS-5 licensed version. How can I use this board with DS-5?

I want to create GCC Linux OS which I can use on the board for booting. Is it possible to create this?

I want to generate the executable using GCC ARM tool chain and use it on the board. For doing this, I can use tool chain from Linaro to generate the executable. For flashing this executable and analyzing the outputs, what tools should I require?