Hi, I have designed a circuit to act as back up power for micro-controller on board in case of power fail which uses TPS63002DRCR.
I have a LTC3225EDDB#TRMPBF super cap charger which charges 2 super caps and brings it to 4.5V. Output of this super cap is given to TPS63002DRCR for generating regulated 5V.
Problem I am facing is, as soon as super cap voltage reaches 1.8V, its stops charging. When I disconnected TPS63002DRCR or disabled it, super cap charged to 4.5V as expected but with TPS63002DRCR it wont charge beyond 1.8V. I read from the datasheet of buck-boost that its output kicks on from 1.8V which i see is the problem. Even if i disconnect the downstream load of buck-boost, it still wont let the super cap charge. Can anybody help me resolve this issue. Thanks.