This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS31HDK : Not responding properly during file open and writing

Hi,


I have functions in the following way:

###############################

main()

{

x1_api();

x2_api();

}

###############################

x1_api() and x2_api() are defined in a library, xapi_lib.a. I just used this library in CCS project and calling procedure is as above.


In x1_api(), I am creating file operations like opening a file, creating a file and writing in to the file etc.

For some part of x1_api() is working fine. Later, board doesnot respond or not able proceed further.

What may be the issue? Can we directly do file i/o operations? These files are created, opened from Debug folder in the project work space.