This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Multi output,Single input

Hey im working on a SIL 2 project which requires 3 masters.

These 3 masters output data independently via Uart/Ethernet.

But out of these 3 outputs,only one input is required at any point of time(selectable by user).

Is there a reliable switch(hardware) that can be used in a SIL 4(yes SIL 4) level project that can choose which data the user requires externally?

Or is there any other means of achieving only 1 out of 3 inputs(software based)?

Note: Im using RM57 for my project.

Thanks