Other Parts Discussed in Thread: HALCOGEN
Hi Sunil,I am facing the same problem in TMS570LS0332x .
In my case 'ERR_ONE_FLG' bit of 'FEDACSTATUS' is set but 'FCOR_ERR_ADD' contain 0x00000000.
I thought of setting some threshold value ( Number single-bit errors that are allowed before an interrupt is generated to the CPU) but it is mentioned in the reference sheet that 'FCOR_ERR_CNT' register is not affected by the EOFEN or EZEFEN error control bits in the FEDACCTRL1 register.
My system gets reset as the ESM pin drives the nERROR pin LOW as this error is occurred.
Can you please tell the reason for this error to occur and what should i do to prevent it.
Thanks