Other Parts Discussed in Thread: TMS570LS20216, OPA4336, OPA2320
Hello,
My project is using TMS570LS20216.
My question is op-amp selection for ADC input.
Actual input range is 0 to +5V and I'm using precision resistor (2K ohm + 3K ohm) to divide input to make 0 to 3V out (REF5030 as reference 3V)
1st try on directly connected condition makes dropped read out value.(4070 for 5V input)
2nd try using OPA4336 as simple current follower makes worse result (more dropped value, max read out not exceed 2500).
3rd try using OPA2320 makes a better result, 3V input that divided from 5V read out is 4088 (4095 desired on 12bit reading).
I can use +5.2V supply only. by this reason, I need to use single supply R2R OP AMP.
What OP AMP can be the best selection?
Thank you.