This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About DMA settings in LCD controller

I am trying a LCD controller of TM4C1299 in raster mode.
However , the color data is not output correctly.
I'm using an external SDRAM as a frame buffer via DMA. So , I suspect that DMA settings are not good .
Could you tell me the DMA settings ?

  • Hello Daisuke

    Do you mean the LCD DMA Settings? Also please share the configuration of the LCD Panel and SDRAM.

    Did you check if the SDRAM Write and Read is correct before starting the LCD?

    Regards
    Amit
  • Hello Amit
    Thanks for your reply.

    I have verified a SDRAM. And I was able to read and write all of the area .
    It is working properly maybe.

    LCD and DMA configuration is as follows:



    /*------------------------------------------------------------------------------
    EPI configuration
    ------------------------------------------------------------------------------*/
    ROM_EPIDividerSet( EPI0_BASE, 0 );

    ROM_EPIModeSet( EPI0_BASE, EPI_MODE_SDRAM );

    ROM_EPIConfigSDRAMSet( EPI0_BASE,
    ui32Freq |
    EPI_SDRAM_FULL_POWER |
    EPI_SDRAM_SIZE_64MBIT,
    1024);

    ROM_EPIAddressMapSet( EPI0_BASE,
    EPI_ADDR_RAM_SIZE_16MB |
    EPI_ADDR_RAM_BASE_6);

    while(HWREG(EPI0_BASE + EPI_O_STAT) &EPI_STAT_INITSEQ);

    /*------------------------------------------------------------------------------
    LCD configuration
    ------------------------------------------------------------------------------*/

    #define SDRAM_GBUF_SIZE (0x00177000)

    uint32_t*pLCDBuf[2];
    pLCDBuf[0] = (uint32_t*)&gwSDRAM[0];
    pLCDBuf[1] = (uint32_t*)&gwSDRAM[SDRAM_GBUF_SIZE];

    tLCDRasterTiming glcdTasterTiming =
    {
    RASTER_TIMING_SYNCS_ON_FALLING_PIXCLK |
    RASTER_TIMING_ACTIVE_HIGH_OE |
    RASTER_TIMING_ACTIVE_HIGH_PIXCLK |
    RASTER_TIMING_ACTIVE_HIGH_HSYNC |
    RASTER_TIMING_ACTIVE_HIGH_VSYNC,
    800, // Screen width
    480, // Screen height
    16, // HFront Porch 1-1024
    160, // HBack Porch1-1024
    80, // HSync Width1-1024
    11, // VFront Porch 0-255
    32, // VBack Porch0-255
    2, // VSync Width1-64
    0 // ACBias Line Count
    };

    // LCD mode
    ROM_LCDModeSet( LCD0_BASE,
    LCD_MODE_RASTER |
    LCD_MODE_AUTO_UFLOW_RESTART,
    30400000, //Pixel clock = 30.4MHz
    ui32SysClock);

    // Output format
    ROM_LCDRasterConfigSet( LCD0_BASE,
    RASTER_FMT_ACTIVE_24BPP_PACKED,
    0);

    // Raster timing
    ROM_LCDRasterTimingSet( LCD0_BASE,
    &glcdTasterTiming);

    // DMA configuration
    ROM_LCDDMAConfigSet( LCD0_BASE,
    LCD_DMA_PRIORITY_3 |
    LCD_DMA_BURST_16 |
    LCD_DMA_BYTE_ORDER_3210 |
    LCD_DMA_FIFORDY_512_WORDS |
    LCD_DMA_PING_PONG );

    // Frame buffer set0
    ROM_LCDRasterFrameBufferSet( LCD0_BASE,
    0,
    pLCDBuf[0],
    0x00177000 ); // 800 * 480 * 32bit / 8 = 1536000 = 0x00177000

    // Frame buffer set1
    ROM_LCDRasterFrameBufferSet( LCD0_BASE,
    1,
    pLCDBuf[1],
    0x00177000 ); // 800 * 480 * 32bit / 8 = 1536000 = 0x00177000

    // Palette set
    ROM_LCDRasterPaletteSet( LCD0_BASE,
    LCD_PALETTE_TYPE_DIRECT,
    (uint32_t *)(pLCDBuf[0]),
    0,
    0,
    0);

    // Raster mode enable
    ROM_LCDRasterEnable(LCD0_BASE);


    Regards
    Daisuke
  • Hello Daisuke

    What is the System Clock Frequency?

    Regards
    Amit
  • Hello Amit

    System clock is 120MHz.
    And configuration is as follows:

    ui32SysClock = ROM_SysCtlClockFreqSet( SYSCTL_XTAL_16MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480, 120000000 );

    Regards
    Daisuke

  • Hello Daisuke

    There are couple of things

    1. The address space of the buffer must map to 0x6000.0000 It is not clear where the buffer gwSDRAM is placed
    2. The EPIDividerSet is using a value of 0 which will result in 120MHz on EPI clock, which is an incorrect setting.

    Regards
    Amit
  • Hello Amit

    Thank you for your advice. I 've checked these.
    But I think both OK.

    gwSDRAM was mapped to 0x6000.0000 certainly.
    And EPIDividerSet is written as follows actually.
    So 2nd parameter is 1.

    if(ui32SysClock > 60000000){ ROM_EPIDividerSet(EPI0_BASE, 1); }
    else { ROM_EPIDividerSet(EPI0_BASE, 0); }

    Are there any things to check?
    It does not affect the prefix "ROM_" of API?

    Regards
    Daisuke
  • Hello Daisuke,

    No, I think the ROM API's would work fine.

    Can you please share the CCS project so that I can debug the same?

    Regards
    Amit
  • Hello Amit,

    I am using the IAR 's development environment , but still ok?
    If you are OK, please tell me how to share the project.
    Could I upload it somewhere?

    Regards
    Daisuke
  • Hello Daisuke,

    IAR project is also fine. You can attach it to the reply post by clicking on "Use rich formatting" on the bottom left.

    Regards
    Amit
  • Hello Amit,

    Here is the my project.

    Please find attached file.

    Regards

    Daisuke

    Monitor.zip

  • Hello Daisuke,

    Which of the two work-spaces do I have to use? Also I found a working code for LCD Raster on a 24bpp panel with SDRAM. You may want to check against this working C file.

    //*****************************************************************************
    //
    // tm4c129_lcdraster_episdram.c - Example demonstrating how to configure the
    //           LCD for raster mode and EPI bus in SDRAM mode for dual buffer
    //           image display
    //
    // Copyright (c) 2014-2015 Texas Instruments Incorporated.  All rights reserved.
    // Software License Agreement
    //
    //   Redistribution and use in source and binary forms, with or without
    //   modification, are permitted provided that the following conditions
    //   are met:
    //
    //   Redistributions of source code must retain the above copyright
    //   notice, this list of conditions and the following disclaimer.
    //
    //   Redistributions in binary form must reproduce the above copyright
    //   notice, this list of conditions and the following disclaimer in the
    //   documentation and/or other materials provided with the
    //   distribution.
    //
    //   Neither the name of Texas Instruments Incorporated nor the names of
    //   its contributors may be used to endorse or promote products derived
    //   from this software without specific prior written permission.
    //
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    //
    // This is part of revision 2.1.1.71 of the Tiva Firmware Development Package.
    //
    //*****************************************************************************
    
    #include <stdbool.h>
    #include <stdint.h>
    #include "inc/hw_epi.h"
    #include "inc/hw_ints.h"
    #include "inc/hw_lcd.h"
    #include "inc/hw_memmap.h"
    #include "inc/hw_types.h"
    #include "inc/hw_gpio.h"
    #include "driverlib/epi.h"
    #include "driverlib/lcd.h"
    #include "driverlib/interrupt.h"
    #include "driverlib/gpio.h"
    #include "driverlib/pin_map.h"
    #include "driverlib/rom.h"
    #include "driverlib/rom_map.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/uart.h"
    #include "utils/uartstdio.h"
    
    //*****************************************************************************
    //
    //! \addtogroup epi_examples_list
    //! <h1>TM4C129 LCD Raster EPI SDRAM Mode (tm4c129_lcdraster_episdram)</h1>
    //!
    //! This example shows how to configure the TM4C129 EPI bus in SDRAM mode and
    //! LCD controller for a 800x480 Raster.  It assumes that a 512Mbit SDRAM is
    //! attached to EPI0.
    //!
    //! For the EPI SDRAM mode, the pinout is as follows:
    //!     Address11:0 - EPI0S11:0
    //!     Bank1:0     - EPI0S14:13
    //!     Data15:0    - EPI0S15:0
    //!     DQML        - EPI0S16
    //!     DQMH        - EPI0S17
    //!     /CAS        - EPI0S18
    //!     /RAS        - EPI0S19
    //!     /WE         - EPI0S28
    //!     /CS         - EPI0S29
    //!     SDCKE       - EPI0S30
    //!     SDCLK       - EPI0S31
    //!
    //! This example uses the following peripherals and I/O signals.  You must
    //! review these and change as needed for your own board:
    //! - EPI0 peripheral
    //! - GPIO Port A peripheral (for EPI0 pins)
    //! - GPIO Port B peripheral (for EPI0 pins)
    //! - GPIO Port C peripheral (for EPI0 pins)
    //! - GPIO Port G peripheral (for EPI0 pins)
    //! - GPIO Port K peripheral (for EPI0 pins)
    //! - GPIO Port L peripheral (for EPI0 pins)
    //! - GPIO Port M peripheral (for EPI0 pins)
    //! - GPIO Port N peripheral (for EPI0 pins)
    //! - EPI0S0  - PK0
    //! - EPI0S1  - PK1
    //! - EPI0S2  - PK2
    //! - EPI0S3  - PK3
    //! - EPI0S4  - PC7
    //! - EPI0S5  - PC6
    //! - EPI0S6  - PC5
    //! - EPI0S7  - PC4
    //! - EPI0S8  - PA6
    //! - EPI0S9  - PA7
    //! - EPI0S10 - PG1
    //! - EPI0S11 - PG0
    //! - EPI0S12 - PM3
    //! - EPI0S13 - PM2
    //! - EPI0S14 - PM1
    //! - EPI0S15 - PM0
    //! - EPI0S16 - PL0
    //! - EPI0S17 - PL1
    //! - EPI0S18 - PL2
    //! - EPI0S19 - PL3
    //! - EPI0S28 - PB3
    //! - EPI0S29 - PN2
    //! - EPI0S30 - PN3
    //! - EPI0S31 - PK5
    //!
    //! The following UART signals are configured only for displaying console
    //! messages for this example.  These are not required for operation of EPI0.
    //! - UART0 peripheral
    //! - GPIO Port A peripheral (for UART0 pins)
    //! - UART0RX - PA0
    //! - UART0TX - PA1
    //!
    //! This example uses the following interrupt handlers.  To use this example
    //! in your own application you must add these interrupt handlers to your
    //! vector table.
    //! - None.
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // Use the following to specify the GPIO pins used by the SDRAM EPI bus.
    //
    //*****************************************************************************
    #define EPI_PORTA_PINS (GPIO_PIN_7 | GPIO_PIN_6)
    #define EPI_PORTB_PINS (GPIO_PIN_3)
    #define EPI_PORTC_PINS (GPIO_PIN_7 | GPIO_PIN_6 | GPIO_PIN_5 | GPIO_PIN_4)
    #define EPI_PORTG_PINS (GPIO_PIN_1 | GPIO_PIN_0)
    #define EPI_PORTK_PINS (GPIO_PIN_5 | GPIO_PIN_3 | GPIO_PIN_2 | GPIO_PIN_1 |   \
                            GPIO_PIN_0)
    #define EPI_PORTL_PINS (GPIO_PIN_3 | GPIO_PIN_2 | GPIO_PIN_1 | GPIO_PIN_0)
    #define EPI_PORTM_PINS (GPIO_PIN_3 | GPIO_PIN_2 | GPIO_PIN_1 | GPIO_PIN_0)
    #define EPI_PORTN_PINS (GPIO_PIN_3 | GPIO_PIN_2)
    
    //*****************************************************************************
    //
    // The starting and ending address for the 64MB SDRAM chip (32Meg x 16bits) on
    // the SDRAM daughter board.
    //
    //*****************************************************************************
    #define SDRAM_START_ADDRESS 0x00000000
    #define SDRAM_END_ADDRESS   0x01FFFFFF
    
    //*****************************************************************************
    //
    // The Mapping address space for the EPI SDRAM.
    //
    //*****************************************************************************
    #define SDRAM_MAPPING_ADDRESS 0x60000000
    
    //*****************************************************************************
    //
    // The define for the LCD Raster Panel BPP, Width and Height
    //
    //*****************************************************************************
    #define RASTER_WIDTH  800
    #define RASTER_HEIGHT 480
    #define SCREEN_BPP    16
    #define SIZE_BUFFER ((RASTER_WIDTH * RASTER_HEIGHT * SCREEN_BPP) / 8)
    
    //*****************************************************************************
    //
    // A pointer to the EPI memory aperture.  Note that g_pui16EPISdram is declared
    // as volatile so the compiler should not optimize reads out of the image.
    //
    //*****************************************************************************
    static volatile uint16_t *g_pui16EPISdram;
    
    //*****************************************************************************
    //
    // Variable for holding the LCD Frame Buffer addres, the frame count, flag to
    // indicate frame buffer change and free frame buffer index
    //
    //*****************************************************************************
    uint32_t *g_pui32DisplayBufferCurr;
    uint32_t g_ui32FrameCounter    = 0;
    volatile bool     g_bFrameBufferChange  = false;
    volatile uint8_t  g_ui8AvailFrameBuffer = 0;
    
    //*****************************************************************************
    //
    // A table used to determine the EPI clock frequency band in use.
    //
    //*****************************************************************************
    typedef struct
    {
        uint32_t ui32SysClock;
        uint32_t ui32FreqFlag;
    }
    tSDRAMFreqMapping;
    
    static tSDRAMFreqMapping g_psSDRAMFreq[] =
    {
        //
        // SysClock >= 100MHz, EPI clock >= 50Mhz (divided by 2)
        //
        {100000000, EPI_SDRAM_CORE_FREQ_50_100},
    
        //
        // SysClock >= 60MHz, EPI clock >= 30MHz (divided by 2)
        //
        {60000000, EPI_SDRAM_CORE_FREQ_50_100},
    
        //
        // SysClock >= 50MHz, EPI clock >= 50MHz (no divider)
        //
        {50000000, EPI_SDRAM_CORE_FREQ_50_100},
    
        //
        // SysClock >= 30MHz, EPI clock >= 30MHz (no divider)
        //
        {50000000, EPI_SDRAM_CORE_FREQ_30_50},
    
        //
        // SysClock >= 15MHz, EPI clock >= 15MHz (no divider)
        //
        {15000000, EPI_SDRAM_CORE_FREQ_15_30},
    
        //
        // SysClock < 15Mhz, EPI clock < 15Mhz (no divider)
        //
        {0, EPI_SDRAM_CORE_FREQ_0_15}
     };
    
    #define NUM_SDRAM_FREQ (sizeof(g_psSDRAMFreq) / sizeof(tSDRAMFreqMapping))
    
    //*****************************************************************************
    //
    // A table used to configure the LCD Panel.
    //
    //*****************************************************************************
    typedef struct
    {
        //
        // A text description of the display mode.
        //
        char *pcMode;
    
        //
        // The required pixel clock for the display mode in Hz.
        //
        uint32_t ui32PixClock;
    
        //
        // The PLL VCO frequency recommended to allow the desired pixel clock
        // frequency to be achieved using an integer system clock divider.
        //
        uint32_t ui32VCOFrequency;
    
        //
        // The recommended system clock frequency to set to allow the pixel clock
        // to be achieved using an integer system clock divider.  Other values are
        // possible so this is merely a recommendation.
        //
        uint32_t ui32SysClockFrequency;
    
        //
        // LCD controller raster display timings for the display mode.
        //
        tLCDRasterTiming sTiming;
    
        //
        // A pointer to an additional, display-specific function which, of not
        // NULL, must be called to perform display initialization prior to
        // enabling the LCD controller raster engine.
        //
        void (*pfnInitDisplay)(uint32_t);
    }
    tRasterDisplayInfo;
    
    const tRasterDisplayInfo g_sOptrex800x480x75Hz =
    {
        "800x480 at 75Hz on Optrex T-55226D043J-LW-A-AAN",
        30000000,
        SYSCTL_CFG_VCO_480,
        120000000,
        {
            (RASTER_TIMING_ACTIVE_HIGH_PIXCLK |
             RASTER_TIMING_SYNCS_ON_RISING_PIXCLK),
    		 RASTER_WIDTH, RASTER_HEIGHT,
            2, 30, 8,
            10, 10, 8,
            0
        },
        0
    };
    
    const tRasterDisplayInfo *g_psDisplayMode = &g_sOptrex800x480x75Hz;
    
    //*****************************************************************************
    //
    // LCD Controller Interrupt Handler
    //
    //*****************************************************************************
    void
    LCD0IntHandler(void)
    {
        uint32_t ui32Status;
    
        //
        // Get the current interrupt status and clear any active interrupts.
        //
        ui32Status = LCDIntStatus(LCD0_BASE, true);
        LCDIntClear(LCD0_BASE, ui32Status);
    
        //
        // If Frame Done interrupt is asserted then check if a new frame
        // is available for updating.
        //
        if(ui32Status & LCD_INT_RASTER_FRAME_DONE)
        {
        	if(!g_bFrameBufferChange)
        	{
            	LCDRasterDisable(LCD0_BASE);
            	MAP_LCDRasterFrameBufferSet(LCD0_BASE, 0, g_pui32DisplayBufferCurr,
                                            SIZE_BUFFER);
                LCDRasterEnable(LCD0_BASE);
    
                //
                // Inform the application that frame buffer has been changed
                //
                g_bFrameBufferChange = true;
            }
        }
    
    
        //
        // If we saw an underflow interrupt, restart the raster.
        //
        if(ui32Status & LCD_INT_UNDERFLOW)
        {
            LCDRasterEnable(LCD0_BASE);
        }
    
    }
    
    //*****************************************************************************
    //
    // LCD controller Display Intiialization function
    //
    //*****************************************************************************
    static void
    DisplayInit(uint32_t ui32SysClkHz)
    {
        //
        // Enable the GPIO peripherals used to interface to the LCD panel.
        //
        MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_LCD0);
        MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
        MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
        MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOJ);
        MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
        MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOQ);
        MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOR);
        MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOS);
        MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOT);
    
        //
        // Configure all the LCD controller pins for hardware control.
        //
        GPIOPinTypeGPIOOutput(GPIO_PORTQ_BASE, GPIO_PIN_5);
        GPIOPinWrite(GPIO_PORTQ_BASE, GPIO_PIN_5, GPIO_PIN_5);
        GPIOPinTypeLCD(GPIO_PORTF_BASE, 0x80);
        GPIOPinTypeLCD(GPIO_PORTJ_BASE, 0x7C);
        GPIOPinTypeLCD(GPIO_PORTN_BASE, 0xC0);
        GPIOPinTypeLCD(GPIO_PORTR_BASE, 0xFF);
        GPIOPinTypeLCD(GPIO_PORTS_BASE, 0xF9);
        GPIOPinTypeLCD(GPIO_PORTT_BASE, 0x0F);
    
        //
        // Set the pin muxing to ensure that LCD signals appear on the required
        // pins.  Note that we take advantage of the fact that we know the mux
        // selector is F here to allow us to OR the value without first masking
        // off anything that may have been there before.
        //
        HWREG(GPIO_PORTF_BASE + GPIO_O_PCTL) |= 0xF0000000;
        HWREG(GPIO_PORTJ_BASE + GPIO_O_PCTL) |= 0x0FFFFF00;
        HWREG(GPIO_PORTN_BASE + GPIO_O_PCTL) |= 0xFF000000;
        HWREG(GPIO_PORTR_BASE + GPIO_O_PCTL) |= 0xFFFFFFFF;
        HWREG(GPIO_PORTS_BASE + GPIO_O_PCTL) |= 0xFFFFF00F;
        HWREG(GPIO_PORTT_BASE + GPIO_O_PCTL) |= 0x0000FFFF;
    
        //
        // Configure the LCD controller for raster operation with a pixel clock
        // as close to the requested pixel clock as possible.
        //
        MAP_LCDModeSet(LCD0_BASE, (LCD_MODE_RASTER | LCD_MODE_AUTO_UFLOW_RESTART),
                       g_psDisplayMode->ui32PixClock, ui32SysClkHz);
    
        //
        // Set the output format for the raster interface.
        //
        MAP_LCDRasterConfigSet(LCD0_BASE, (RASTER_FMT_ACTIVE_PALETTIZED_16BIT |
                               RASTER_NIBBLE_MODE_ENABLED |
                               RASTER_READ_ORDER_REVERSED), 0);
    
    
        MAP_LCDRasterTimingSet(LCD0_BASE, &(g_psDisplayMode->sTiming));
    
        //
        // Configure DMA-related parameters.
        //
        MAP_LCDDMAConfigSet(LCD0_BASE, LCD_DMA_BURST_16 | LCD_DMA_FIFORDY_64_WORDS);
    
        //
        // If the chosen display has an initialization function, call it now.
        //
        if(g_psDisplayMode->pfnInitDisplay)
        {
            g_psDisplayMode->pfnInitDisplay(ui32SysClkHz);
        }
    
        //
        // Set up the frame buffer.  Note that we allow this buffer to extend
        // outside the available SRAM.  This allows us to easily test modes where
        // we can't fit the whole frame in memory, realizing, of course, that
        // part of the display will contain crud.
        //
        MAP_LCDRasterFrameBufferSet(LCD0_BASE, 0, g_pui32DisplayBufferCurr,
                                    SIZE_BUFFER);
    
        //
        // Enable the LCD interrupts.
        //
        MAP_LCDIntEnable(LCD0_BASE, (LCD_INT_DMA_DONE | LCD_INT_SYNC_LOST |
                         LCD_INT_UNDERFLOW | LCD_INT_RASTER_FRAME_DONE | LCD_INT_EOF0));
    
        MAP_IntEnable(INT_LCD0);
    
        //
        // Enable the raster output.
        //
        MAP_LCDRasterEnable(LCD0_BASE);
    }
    //*****************************************************************************
    //
    // This function sets up UART0 to be used for a console to display information
    // as the example is running.
    //
    //*****************************************************************************
    void
    InitConsole(void)
    {
        //
        // Enable GPIO port A which is used for UART0 pins.
        // TODO: change this to whichever GPIO port you are using.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
    
        //
        // Configure the pin muxing for UART0 functions on port A0 and A1.
        // This step is not necessary if your part does not support pin muxing.
        // TODO: change this to select the port/pin you are using.
        //
        GPIOPinConfigure(GPIO_PA0_U0RX);
        GPIOPinConfigure(GPIO_PA1_U0TX);
    
        //
        // Enable UART0 so that we can configure the clock.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
    
        //
        // Use the internal 16MHz oscillator as the UART clock source.
        //
        UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
    
        //
        // Select the alternate (UART) function for these pins.
        // TODO: change this to select the port/pin you are using.
        //
        GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
    
        //
        // Initialize the UART for console I/O.
        //
        UARTStdioConfig(0, 115200, 16000000);
    }
    
    //*****************************************************************************
    //
    // Create a barrel shifter to move the final image pixel to be shown on the
    // screen
    //
    //*****************************************************************************
    void
    GetBarrelValue(uint16_t *pui16Value)
    {
    	switch(*pui16Value)
    	{
    		case 0x001F:
    			*pui16Value = 0x003E;
    			break;
    		case 0x003E:
    			*pui16Value = 0x007C;
    			break;
    		case 0x007C:
    			*pui16Value = 0x00F8;
    			break;
    		case 0x00F8:
    			*pui16Value = 0x01F0;
    			break;
    		case 0x01F0:
    			*pui16Value = 0x03E0;
    			break;
    		case 0x03E0:
    			*pui16Value = 0x07C0;
    			break;
    		case 0x07C0:
    			*pui16Value = 0x0F80;
    			break;
    		case 0x0F80:
    			*pui16Value = 0x1F00;
    			break;
    		case 0x1F00:
    			*pui16Value = 0x3E00;
    			break;
    		case 0x3E00:
    			*pui16Value = 0x7C00;
    			break;
    		case 0x7C00:
    			*pui16Value = 0xF800;
    			break;
    		case 0xF800:
    			*pui16Value = 0xF001;
    			break;
    		case 0xF001:
    			*pui16Value = 0xE003;
    			break;
    		case 0xE003:
    			*pui16Value = 0xC007;
    			break;
    		case 0xC007:
    			*pui16Value = 0x800F;
    			break;
    		case 0x800F:
    			*pui16Value = 0x001F;
    			break;
    		default:
    			*pui16Value = 0x001F;
    			break;
    	}
    }
    
    //*****************************************************************************
    //
    // Configure EPI0 in SDRAM mode.  The EPI memory space is setup using an a
    // simple C array.  This example shows how to read and write to an SDRAM card
    // using the EPI bus in SDRAM mode.
    //
    //*****************************************************************************
    int
    main(void)
    {
        uint32_t ui32Val, ui32Freq, ui32SysClock;
        uint16_t ui16BarrelLoad = 0x001F;
    
        //
        // Set the clocking to run at 120MHz from the PLL.
        // TODO: Update this call to set the system clock frequency your
        // application requires.
        //
        ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL |
                                          SYSCTL_CFG_VCO_480), 120000000);
    
        //
        // Set up the serial console to use for displaying messages.  This is
        // just for this example program and is not needed for EPI operation.
        //
        InitConsole();
    
        g_ui32FrameCounter = 0;
    
        //
        // Display the setup on the console.
        //
        UARTprintf("EPI SDRAM Mode ->\n");
        UARTprintf("  Type: SDRAM\n");
        UARTprintf("  Starting Address: 0x%08x\n", SDRAM_MAPPING_ADDRESS);
        UARTprintf("  End Address: 0x%08x\n",
                   (SDRAM_MAPPING_ADDRESS + SDRAM_END_ADDRESS));
        UARTprintf("  Data: 16-bit\n");
        UARTprintf("  Size: 64MB (32Meg x 16bits)\n\n");
    
        //
        // The EPI0 peripheral must be enabled for use.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_EPI0);
    
        //
        // For this example EPI0 is used with multiple pins on PortA, B, C, G, H,
        // K, L, M and N.  The actual port and pins used may be different on your
        // part, consult the data sheet for more information.
        // TODO: Update based upon the EPI pin assignment on your target part.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOK);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOL);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOM);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
    
        //
        // This step configures the internal pin muxes to set the EPI pins for use
        // with EPI.  Please refer to the datasheet for more information about pin
        // muxing.  Note that EPI0S27:20 are not used for the EPI SDRAM
        // implementation.
        // TODO: Update this section based upon the EPI pin assignment on your
        // target part.
        //
    
        //
        // EPI0S4 ~ EPI0S7: C4 ~ 7
        //
        ui32Val = HWREG(GPIO_PORTC_BASE + GPIO_O_PCTL);
        ui32Val &= 0x0000FFFF;
        ui32Val |= 0xFFFF0000;
        HWREG(GPIO_PORTC_BASE + GPIO_O_PCTL) = ui32Val;
    
        //
        // EPI0S8 ~ EPI0S9: A6 ~ 7
        //
        ui32Val = HWREG(GPIO_PORTA_BASE + GPIO_O_PCTL);
        ui32Val &= 0x00FFFFFF;
        ui32Val |= 0xFF000000;
        HWREG(GPIO_PORTA_BASE + GPIO_O_PCTL) = ui32Val;
    
        //
        // EPI0S10 ~ EPI0S11: G0 ~ 1
        //
        ui32Val = HWREG(GPIO_PORTG_BASE + GPIO_O_PCTL);
        ui32Val &= 0xFFFFFF00;
        ui32Val |= 0x000000FF;
        HWREG(GPIO_PORTG_BASE + GPIO_O_PCTL) = ui32Val;
    
        //
        // EPI0S12 ~ EPI0S15: M0 ~ 3
        //
        ui32Val = HWREG(GPIO_PORTM_BASE + GPIO_O_PCTL);
        ui32Val &= 0xFFFF0000;
        ui32Val |= 0x0000FFFF;
        HWREG(GPIO_PORTM_BASE + GPIO_O_PCTL) = ui32Val;
    
        //
        // EPI0S16 ~ EPI0S19: L0 ~ 3
        //
        ui32Val = HWREG(GPIO_PORTL_BASE + GPIO_O_PCTL);
        ui32Val &= 0xFFFF0000;
        ui32Val |= 0x0000FFFF;
        HWREG(GPIO_PORTL_BASE + GPIO_O_PCTL) = ui32Val;
    
        //
        // EPI0S28 : B3
        //
        ui32Val = HWREG(GPIO_PORTB_BASE + GPIO_O_PCTL);
        ui32Val &= 0xFFFF0FFF;
        ui32Val |= 0x0000F000;
        HWREG(GPIO_PORTB_BASE + GPIO_O_PCTL) = ui32Val;
    
        //
        // EPI0S29 ~ EPI0S30: N2 ~ 3
        //
        ui32Val = HWREG(GPIO_PORTN_BASE + GPIO_O_PCTL);
        ui32Val &= 0xFFFF00FF;
        ui32Val |= 0x0000FF00;
        HWREG(GPIO_PORTN_BASE + GPIO_O_PCTL) = ui32Val;
    
        //
        // EPI0S00 ~ EPI0S03, EPI0S31 : K0 ~ 3, K5
        //
        ui32Val = HWREG(GPIO_PORTK_BASE + GPIO_O_PCTL);
        ui32Val &= 0xFF0F0000;
        ui32Val |= 0x00F0FFFF;
        HWREG(GPIO_PORTK_BASE + GPIO_O_PCTL) = ui32Val;
    
        //
        // Configure the GPIO pins for EPI mode.  All the EPI pins require 8mA
        // drive strength in push-pull operation.  This step also gives control of
        // pins to the EPI module.
        //
        GPIOPinTypeEPI(GPIO_PORTA_BASE, EPI_PORTA_PINS);
        GPIOPinTypeEPI(GPIO_PORTB_BASE, EPI_PORTB_PINS);
        GPIOPinTypeEPI(GPIO_PORTC_BASE, EPI_PORTC_PINS);
        GPIOPinTypeEPI(GPIO_PORTG_BASE, EPI_PORTG_PINS);
        GPIOPinTypeEPI(GPIO_PORTK_BASE, EPI_PORTK_PINS);
        GPIOPinTypeEPI(GPIO_PORTL_BASE, EPI_PORTL_PINS);
        GPIOPinTypeEPI(GPIO_PORTM_BASE, EPI_PORTM_PINS);
        GPIOPinTypeEPI(GPIO_PORTN_BASE, EPI_PORTN_PINS);
    
        //
        // Is our current system clock faster than we can drive the SDRAM clock?
        //
        if(ui32SysClock > 60000000)
        {
            //
            // Yes. Set the EPI clock to half the system clock.
            //
            EPIDividerSet(EPI0_BASE, 1);
        }
        else
        {
            //
            // With a system clock of 60MHz or lower, we can drive the SDRAM at
            // the same rate so set the divider to 0.
            //
            EPIDividerSet(EPI0_BASE, 0);
        }
    
        //
        // Sets the usage mode of the EPI module.  For this example we will use
        // the SDRAM mode to talk to the external 64MB SDRAM daughter card.
        //
        EPIModeSet(EPI0_BASE, EPI_MODE_SDRAM);
    
        //
        // Keep the compiler happy by setting a default value for the frequency
        // flag.
        //
        ui32Freq = g_psSDRAMFreq[NUM_SDRAM_FREQ - 1].ui32FreqFlag;
    
        //
        // Examine the system clock frequency to determine how to set the SDRAM
        // controller's frequency flag.
        //
        for(ui32Val = 0; ui32Val < NUM_SDRAM_FREQ; ui32Val++)
        {
            //
            // Is the system clock frequency above the break point in the table?
            //
            if(ui32SysClock >= g_psSDRAMFreq[ui32Val].ui32SysClock)
            {
                //
                // Yes - remember the frequency flag to use and exit the loop.
                //
                ui32Freq = g_psSDRAMFreq[ui32Val].ui32FreqFlag;
                break;
            }
        }
    
        //
        // Configure the SDRAM mode.  We configure the SDRAM according to our core
        // clock frequency.  We will use the normal (or full power) operating
        // state which means we will not use the low power self-refresh state.
        // Set the SDRAM size to 64MB with a refresh interval of 1024 clock ticks.
        //
        EPIConfigSDRAMSet(EPI0_BASE, (ui32Freq | EPI_SDRAM_FULL_POWER |
                          EPI_SDRAM_SIZE_512MBIT), 468);
    
        //
        // Set the address map.  The EPI0 is mapped from 0x60000000 to 0x01FFFFFF.
        // For this example, we will start from a base address of 0x60000000 with
        // a size of 256MB.  Although our SDRAM is only 64MB, there is no 64MB
        // aperture option so we pick the next larger size.
        //
        EPIAddressMapSet(EPI0_BASE, EPI_ADDR_RAM_SIZE_256MB | EPI_ADDR_RAM_BASE_6);
    
        //
        // Wait for the SDRAM wake-up to complete by polling the SDRAM
        // initialization sequence bit.  This bit is true when the SDRAM interface
        // is going through the initialization and false when the SDRAM interface
        // it is not in a wake-up period.
        //
        while(HWREG(EPI0_BASE + EPI_O_STAT) &  EPI_STAT_INITSEQ)
        {
        }
    
        //
        // Set the EPI memory pointer to the base of EPI memory space.  Note that
        // g_pui16EPISdram is declared as volatile so the compiler should not
        // optimize reads out of the memory.  With this pointer, the memory space
        // is accessed like a simple array.
        //
        g_pui16EPISdram = (uint16_t *)0x60000000;
    
        //
        // Read the initial data in SDRAM, and display it on the console.
        //
        UARTprintf("  SDRAM Initial Data:\n");
        UARTprintf("     Mem[0x6000.0000] = 0x%4x\n",
                   g_pui16EPISdram[SDRAM_START_ADDRESS]);
        UARTprintf("     Mem[0x6000.0001] = 0x%4x\n",
                   g_pui16EPISdram[SDRAM_START_ADDRESS + 1]);
        UARTprintf("     Mem[0x603F.FFFE] = 0x%4x\n",
                   g_pui16EPISdram[SDRAM_END_ADDRESS - 1]);
        UARTprintf("     Mem[0x603F.FFFF] = 0x%4x\n\n",
                   g_pui16EPISdram[SDRAM_END_ADDRESS]);
    
        //
        // Display what writes we are doing on the console.
        //
        UARTprintf("  SDRAM Write:\n");
        UARTprintf("     Mem[0x6000.0000] <- 0xabcd\n");
        UARTprintf("     Mem[0x6000.0001] <- 0x1234\n");
        UARTprintf("     Mem[0x603F.FFFE] <- 0xdcba\n");
        UARTprintf("     Mem[0x603F.FFFF] <- 0x4321\n\n");
    
        //
        // Write to the first 2 and last 2 address of the SDRAM card.  Since the
        // SDRAM card is word addressable, we will write words.
        //
        g_pui16EPISdram[SDRAM_START_ADDRESS] = 0xabcd;
        g_pui16EPISdram[SDRAM_START_ADDRESS + 1] = 0x1234;
        g_pui16EPISdram[SDRAM_END_ADDRESS - 1] = 0xdcba;
        g_pui16EPISdram[SDRAM_END_ADDRESS] = 0x4321;
    
        //
        // Read back the data you wrote, and display it on the console.
        //
        UARTprintf("  SDRAM Read:\n");
        UARTprintf("     Mem[0x6000.0000] = 0x%4x\n",
                   g_pui16EPISdram[SDRAM_START_ADDRESS]);
        UARTprintf("     Mem[0x6000.0001] = 0x%4x\n",
                   g_pui16EPISdram[SDRAM_START_ADDRESS + 1]);
        UARTprintf("     Mem[0x603F.FFFE] = 0x%4x\n",
                   g_pui16EPISdram[SDRAM_END_ADDRESS - 1]);
        UARTprintf("     Mem[0x603F.FFFF] = 0x%4x\n\n",
                   g_pui16EPISdram[SDRAM_END_ADDRESS]);
    
        //
        // Check the validity of the data.
        //
        if((g_pui16EPISdram[SDRAM_START_ADDRESS] == 0xabcd) &&
           (g_pui16EPISdram[SDRAM_START_ADDRESS + 1] == 0x1234) &&
           (g_pui16EPISdram[SDRAM_END_ADDRESS - 1] == 0xdcba) &&
           (g_pui16EPISdram[SDRAM_END_ADDRESS] == 0x4321))
        {
            //
            // Read and write operations were successful.  Return with no errors.
            //
            UARTprintf("Read and write to external SDRAM was successful!\n");
        }
        else
        {
            //
            // Display on the console that there was an error.
            //
            UARTprintf("Read and/or write failure!");
            UARTprintf(" Check if your SDRAM card is plugged in.");
            while(1)
            {
            }
        }
    
        //
        // Frame buffer 1 is assigned already to have the first image and set the
        // flag that the next buffer is ready for a new image
        //
        g_ui8AvailFrameBuffer    = 2;
        g_bFrameBufferChange     = true;
    
        //
        // Set the address of the first frame buffer
        //
        g_pui32DisplayBufferCurr = (uint32_t *)g_pui16EPISdram;
    
        //
        // Fill the SDRAM with the frame buffer pixel color
        //
        for(ui32Val=0; ui32Val < SIZE_BUFFER; ui32Val++)
        {
        	g_pui16EPISdram[SDRAM_START_ADDRESS + ui32Val] = ui16BarrelLoad;
        }
    
        //
        // Initialize the Display and put out the first image
        //
        DisplayInit(ui32SysClock);
    
        //
        // Read and/or write operations were unsuccessful.  Wait in while(1) loop
        // for debugging.
        //
        while(1)
        {
        	//
        	// Barrel Shift the current pixel value
        	//
        	GetBarrelValue(&ui16BarrelLoad);
    
        	//
        	// Wait for the LCD interrupt handler to tell the application that the
        	// last frame buffer has been loaded and it has freed up the previous
        	// frame buffer being used
        	//
        	while(!g_bFrameBufferChange);
    
        	//
        	// Check which frame buffer is free and populate it with the new pixel
        	// value
        	//
        	if(g_ui8AvailFrameBuffer == 1)
        	{
        	    for(ui32Val=0; ui32Val < SIZE_BUFFER; ui32Val++)
        	    {
        	    	g_pui16EPISdram[SDRAM_START_ADDRESS + ui32Val] = ui16BarrelLoad;
        	    	SysCtlDelay(30);
        	    }
    
        	    g_ui8AvailFrameBuffer    = 2;
        	    g_pui32DisplayBufferCurr = (uint32_t *)g_pui16EPISdram;
        	}
        	else if(g_ui8AvailFrameBuffer == 2)
        	{
        	    for(ui32Val=0; ui32Val < SIZE_BUFFER; ui32Val++)
        	    {
        	    	g_pui16EPISdram[SDRAM_START_ADDRESS + SIZE_BUFFER + ui32Val] = ui16BarrelLoad;
        	    	SysCtlDelay(30);
        	    }
    
        	    g_ui8AvailFrameBuffer    = 1;
        	    g_pui32DisplayBufferCurr = (uint32_t *)g_pui16EPISdram + (SIZE_BUFFER/2);
        	}
    
        	//
        	// Set the flag for the interrupt handle that buffer change is complete
        	// and the next image buffer is available
        	//
        	g_bFrameBufferChange = false;
        }
    }
    

    Regards

    Amit

  • Hello Amit,

    >Which of the two work-spaces do I have to use?

    Monitorworkspace.eww is.
    It is the overall workspace that contains the tiva libraries.
    Monitor.eww is just a sub-workspace.

    >You may want to check against this working C file.
    Okey, I'll check it.

    Regards
    Daisuke

  • Hello Amit,

    It worked fine.
    It seems DMA configuration was not good.
    Thank you , Boss has very pleased.

    Regards
    Daisuke

  • Amit Ashara said:
    attach it to the reply post by clicking on "Use rich formatting" on the bottom left.

    Cb1 staffers (gleefully) note that cb1 (more than once) has made that same "left/right" transposition...   Rich is to the right - as is "proper" politics...