Hello,
I need to obtain the temperature value from temperature sensor available on TMDSRM48USB kit.
I need to transmit the temperature continuously on Terminal/SCILIN port.
I am able to obtain some value from ADC but its not exact.
I want to display upto 2 digits after decimal. I have a rough code taken from light sensor.
@file sys_main.c
/* USER CODE BEGIN (0) */
#include "sci.h"
#include "adc.h"
#include "stdlib.h"
/* USER CODE END */
/* Include Files */
#include "sys_common.h"
#include "system.h"
/* USER CODE BEGIN (1) */
unsigned char command[8];
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
void cal_Temp(void);
/* USER CODE END */
void main(void)
{
/* USER CODE BEGIN (3) */
sciInit();
adcInit();
while(1){
cal_Temp();
}
/* USER CODE END */
}
/* USER CODE BEGIN (4) */
void cal_Temp(void){
adcData_t adc_data ; //ADC data structure
adcData_t *adc_data_ptr = &adc_data;
unsigned char NumberOfChars ,value;
adcStartConversion(adcREG1,adcGROUP1);
while(!adcIsConversionComplete(adcREG1,adcGROUP1)); //wait for adc conversion
adcGetData(adcREG1,1U,adc_data_ptr); //store conversion into pointer
value = (unsigned int) adc_data_ptr->value;
NumberOfChars= ltoa(value, (char *)command);
sciSend(scilinREG,NumberOfChars,command);
sciSend(scilinREG,2,(unsigned char*)"\r\n");
}
/* USER CODE END */