This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Pin F0 strange behavior due to NMI on TM4C?

I already solved one problem with tricky pin F0, getting some help here to disable NMI. Now it seems there is another problem. I am using this pin to operate a relay, and whenever my program stops, NMI is re-enabled, F0 goes high (I think - going to test with a scope tomorrow) and the relay is closed.

Here's the code I'm using:

	ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);	// Pins: RGB LED, Relays
	
	ROM_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);	// RGB LED

	// Port F unlock procedure:
	HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;		// Unlock the port
	HWREG(GPIO_PORTF_BASE + GPIO_O_CR) |= GPIO_PIN_0;		// Unlock the pin
	HWREG(GPIO_PORTF_BASE + GPIO_O_AFSEL) &= ~GPIO_PIN_0;  
	HWREG(GPIO_PORTF_BASE + GPIO_O_DEN) |= GPIO_PIN_0;
	HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = 0;			// Lock the port

	// Then turn it on:
	ROM_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_0);		// Rel1 (conflict with USR SW2)

Am I doing something wrong? Is there something else I should be doing to keep my relay from closing each time the program runs?