This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB Demodulator usin tm4c123 development board



In advance I'm not embedded systems engineer , so 

I have a MAX2112 DVB-S2 tuner and its circuit , its output are i+ , i- , q+ , q- , now I should take these outputs and the i2c two wires to demodulator , then to DSP chip , but in fact i'm interested in Software Defined Radio so taking these outputs to something in between the pc host and the Tuner(MAX2112 circuit) ,so I use TI tm4c123 it has many analog inputs and ADC pins ----------- my question------- is that configuration right for upstreaming the demodulated signal on the USB 2.0 port to the host pc ?

thanks in advance .