This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

flash bootloader and TI-RTOS

Hello,

 We are thinking of developing a flash boot-loader to do power on self test before a TI-RTOS application is started and firmware upgrade. Can we use TI-RTOS drivers in the flash boot-loader or should we use only tivaware APIs

TM4C129NCZAD microcontroller based custom board , with TI-RTOS 2,14, tivaware 2.1.1.71.

Thanks in Advance

Narendra

  • Hello Narendra,

    You may develop the boot loader using TI RTOS, but the memory footprint of TI RTOS for a boot loader would be far much more than bare metal TivaWare APIs. Also I do not have much experience with TI RTOS boot loader, so you may have to wait for other folks to help you out as well.

    Regards
    Amit