I am using the DK-TM4129x, and I want to use a timer that is in PWM mode to trigger the DMA. This question came up more than 3 years ago (I tried to paste the link and the interface went crazy, sorry). The answer at that time (per Stellaris Joe) was that this is not possible. Now there is new silicon, new datasheets (clearly states that this is possible), and new errata, and none of these mention that this is still an issue, so it would seem to be wrong to assume that this problem has not been fixed already.
So, can anybody confirm that this is possible? I am trying and I think I have all the settings correctly. I have done a lot of DMA programming over the years with LM3S and now TM4C devices, and I can't see that I'm doing anything wrong. If someone can confirm that this is indeed possible, or not possible, that would be a great help.
Dustin