This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Switching RM48 Micro controller through software codes



Hello,

i need to switch ON/OFF the RM48 Micro controller through software codes when power supply is online.

Is it possible do this task. How it can be done. 

  • Manjunathan,

    Here is what is possible with just the RM48 itself:
    1) you can switch off power internally to modules that you are not using, but this has only a small effect on power consumption.
    see SPNU503b chapter 3 PMM power management module.
    2) There are some low power modes that stop the clocks which reduces dynamic power consumption.
    see SPNU503b chapter 2 section 2.4.3 and note that there is a static leakage portion of the device
    power consumption that can be significant at high temperature.

    -Anthony
  • Thank you Sir,

    I will check.