Other Parts Discussed in Thread: TPS54426, TPS2411, LM2585
Greetings E2E Community
I am experiencing permanent failures of the humidity and pressure sensors of the booster pack at random occasions. The booster pack is used to monitor the state (temperature, humidity and orientation) of a sealed underwater vehicle. Typical conditions of the vehicle's sealed environment are temperatures ranging from 0C to 30C and a pressure of about 1 atmosphere.
Diagnostic test are performed on the vehicle before deployments and after recovery to assess its working state. In addition a log of the sensor readings is kept during deployments on a SD card.
At random occasions when performing a pre-deployment diagnostic test or normal bench test of the vehicle the pressure or humidity sensor would fail. This has happened on three separate occasions with 3 different vehicles and three separate booster packs. The pressure sensor has failed once, exhibiting sporadic readings, usually in the upper range of the sensors capabilities. and the humidity sensors have failed twice, exhibiting constant readings, regardless of changing environmental temperatures.
The power supply of the 3.3V rail of the vehicle is powered by a TPS54426 buck switching converter, with an average output of 3.36V. The environmental and electrical characteristics of the operating environment are withing acceptable ranges for both sensors and no other sensors in the booster pack have exhibited these failures.
Since the failures are exhibited between power on-off cycles of the vehicle I suspect the failures have something to do with a transient voltage in the power supplies, but I am no entirely sure and currently investigating. I am writing to see if someone has experienced these failures before or if someone has any insight on the problem. Any advice is greatly appreciated and thanks, in advance for your time.