Other Parts Discussed in Thread: ENERGIA
I am uploading the Fade example of energia to the connected launchpad.
But the LED is not fading, it is just blinking.
I tried other pins also like PF3 and PG0 and I checked the output using a multimeter since I don't have an oscilloscope. But the output is about 2.7v and not reducing.
*/
int brightness = 0; // how bright the LED is
int fadeAmount = 5; // how many points to fade the LED by
void setup() {
// declare pin 14 to be an output:
pinMode(GREEN_LED, OUTPUT);
}
void loop() {
// set the brightness of pin 9:
analogWrite(GREEN_LED, brightness);
// change the brightness for next time through the loop:
brightness = brightness + fadeAmount;
// reverse the direction of the fading at the ends of the fade:
if (brightness == 0 || brightness == 255) {
fadeAmount = -fadeAmount ;
}
// wait for 30 milliseconds to see the dimming effect
delay(30);
}