Other Parts Discussed in Thread: ENERGIA
Hi everyone!
First, this is my first post on the forum and programming a micro-controller. I'm working on a independent school project using the Tiva TM4C123G and Matlab 2015b on Ubuntu 15.04. I have tried to get Matlab to communicate with the board but it is only unidirectional. I mean the board can read the data I send from Matlab but Matlab can't read the data send from the board. At the moment of using fscanf(s,'%d') (s being the serial port object) Matlab returns the following:
Warning: Unsuccessful read: A timeout occurred before the Terminator was reached..
Nevertheless, the board still reads the data sent from Matlab. I programmed the board using Energia with the following code:
#define LED_G GREEN_LED
#define LED_B BLUE_LED
#define LED_R RED_LED
int temp;
int matlabData; // integer sent from Matlab
void setup()
{
// put your setup code here, to run once:
pinMode(LED_G, OUTPUT);
pinMode(LED_B, OUTPUT);
pinMode(LED_R, OUTPUT);
Serial.begin(9600);
delay(100);
}
void loop()
{
// put your main code here, to run repeatedly:
while (Serial.available() == 0)
{
}
if(Serial.available()>0)
{
matlabData = Serial.read();
if(matlabData == 1)
{
digitalWrite(LED_G, HIGH);
digitalWrite(LED_B, LOW);
digitalWrite(LED_R, LOW);
temp = 1;
Serial.println(temp);
delay(10);
}
else if(matlabData == 2)
{
digitalWrite(LED_B, HIGH);
digitalWrite(LED_G, LOW);
digitalWrite(LED_R, LOW);
temp = 2;
Serial.println(temp);
delay(10);
}
else if(matlabData == 3)
{
digitalWrite(LED_R, HIGH);
digitalWrite(LED_B, LOW);
digitalWrite(LED_G, LOW);
temp = 3;
Serial.println(temp);
delay(10);
}
}
else
{
digitalWrite(LED_B, LOW);
digitalWrite(LED_G, LOW);
digitalWrite(LED_R, LOW);
}
}
The code is just basic stuff to play with the on-board LED and test the communication.
On Matlab's side I wrote:
To set the communication:
function[obj,flag] = setupSerial(comPort) flag = 1; % Initialize Serial object obj = serial(comPort); set(obj,'DataBits',8); set(obj,'StopBits',1); set(obj,'BaudRate',9600); set(obj,'Parity','none'); % set(obj,'InputBufferSize',1000); fopen(obj); fscanf(obj,'%u'); end
and the main:
clear all;
close all;
clc;
port = '/dev/ttyACM0'
if (~exist('serialFlag','var'))
[s,flag] = setupSerial(port);
end
answer = 1;
while answer
answer = input('0,1,2,3: ');
fprintf(s,char(answer));
output = fscanf(s,'%d')
end
closeSerial;
closeSerial just closes and remove the port. I have tried for a few days but I can't figure out why it doesn't work. It would be great if someone has an idea how to solve this. Thank you very much in advance. :)