Hi,
When I do file I/O operations i.e. file read/write from the board, I am able to do from the Debug folder.
Is there any way that I can access through the SDCard which is present on the board?
Time taken to read/write to the Debug folder from the board is more.
Is there any better option so that I can optimize the time taken for file i/o operations?
Thanks and Regards
Sridhar Artham