This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Configuring Timer in Tiva Lauchpad

Hi

I have a problem with EK-TM4C1294 TIVA LAUNCHPAD.

I am configuring the timer0 as periodic, 32 bits of 1s and I want polling not by interruption, but I haven´t the period correct.

This is my code

TIMER_A = 120000000;

void Conf_timer_periodico(void)
{

ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0); //Enable the peripheral

ROM_TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC); //Configure 32-bit periodic timer (down count)

ROM_TimerLoadSet(TIMER0_BASE, TIMER_A, g_ui32SysClock);
ROM_TimerEnable(TIMER0_BASE, TIMER_A); // Enable the timer

return;

}

main

{

// Run from the PLL at 120 MHz.
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN | SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);

while(1)
{

if  ((TimerValueGet (TIMER0_BASE, TIMER_TIMA_TIMEOUT)) == 0x00)
{

TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT)

GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, GPIO_PIN_1); //ON LED1

}

}

}

Please help me.